选择版本

选择版本

未找到结果。请清除搜索,并重试。

PROCESSOR-SDK-LINUX-K2G

适用于 K2Gx 的 Linux 处理器 SDK

选择版本
未找到结果。请清除搜索,并重试。
版本: 04.01.00.06
发布日期: 25 九月 2017

Code Composer Studio IDE for Windows Host

Code Composer Studio IDE for Linux Host

Only used when creating an SD Card on Windows

MD5 校验和

Standalone Linaro Toolchain - Linaro GCC 6.2.1 2016.11 hard-float toolchain

K2G Linux SDK prebuilt BSP binaries and root filesystem

MD5 校验和

K2G Linux SDK Arago source downloads

MD5 校验和

Quick Start Guide that was included in the EVM kit

文档

Instructions for creating an SD Card with Linux

Instructions for creating an SD Card with Windows

Software Manifest of Components Inside the SDK

发布信息

Thank you for your interest in the K2G Software Development Kit (SDK). If you would like to install the full SDK on a Linux Host computer for development, you'll need the K2G Linux SDK Essentials below. If you would like to evaluate the SDK by running it on one of the below platforms and you prefer not to install the full SDK at this time, please see the K2G Linux SDK SD Card Creation section below.

More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .