选择版本

选择版本

未找到结果。请清除搜索,并重试。

GASGAUGECHEM-SW

电量监测计化学物更新器

选择版本
未找到结果。请清除搜索,并重试。
版本: 935
发布日期: 29 十二月 2021

Gas Gauge Chemistry Updater installer(Windows only) for bq Evaluation/bqEasy

MD5 校验和

Use this file with Battery Management Studio (bqStudio) Help menu to import the latest chemistries.

MD5 校验和
产品
电池电量监测
BQ20Z40-R1 采用 Impedance Track™ 技术且符合 SBS 1.1 标准的电量监测计 BQ20Z70-V160 采用 Impedance Track™ 技术且符合 SBS 1.1 标准的电量监测计,可与 bq29330 一起使用 BQ20Z80A-V110 采用 Impedance Track™ 技术且符合 SBS 1.1 标准的电量监测计,可与 bq29312A 一起使用 BQ27505-J2 系统侧 Impedance Track™ 电量监测计,固件版本为 v2.15 BQ27505-J3 系统侧 Impedance Track™ 电量监测计,固件版本为 v2.20 BQ27505-J4 系统侧 Impedance Track™ 电量监测计,固件版本为 v2.24
硬件开发
BQEVSW 适用于 bq30z554-R1 的 bq 评估软件 (bqEVSW) v0.0.92

文档

Gas gauge Chemistry updater Documentation

最新动态

The Gas Gauge Chemistry Updater contains new chemistry IDs that have been characterized.

Please refer to the Chemistry ID history for the list of Chemistry IDs added in this release.

发布信息

Important Note: The latest chemistry updater for bqStudio requires bqStudio 1.3.86 or higher.

Instructions for bqStudio Chemistry database update:

  • 1. Download the "bqStudio Chemistry Update zip" file and save with extension *.zip
  • 2. Connect an impedance track(IT) enabled gauge to the PC and open Battery Management Studio(bqStudio). bqStudio must autodetect the gauge. Alternatively select impedance track enabled gauge from selection list.
  • 3. From bqStudio "Help" menu select "Update Chemistry". When prompted point bqStudio to the downloaded zip file. Upon successful update, a confirmation message will be shown.
  • Instructions for bqEVSW Chemistry database update:

  • Run the installer to update the chemistry database used by bq Evaluation / bqEasy software
  • Step by step instructions for bqStudio and bqEVSW