Forward Annotation
                               ------------------

                        02:05 PM Tuesday, March 11, 2014
Job Name: D:\PCB Projects\Expedition\Nanopower\EVM\ADS704x_SE_EVM\PCB\ADS704x_SE_EVM.pcb


Version:  01.01.00

     The PDBs listed in the project file will be searched to satisfy the parts
      requirements of the CDB and to refresh with newer data any duplicates found in the
      Target PDB.

     The schematic source is a Common Data Base.

     The AllowAlphaRefDes status indicates that reference
      designators containing all alpha characters should be deleted
      and the relevant symbols repackaged.

     The FLATNETNAMEs status indicates that the present set
      of schematic netnames should be used to update the
      FLATNETNAMEs.

     The present Common DataBase is up to date with the schematic
      source files.

     Common Data Base has been read

     Target PDB Name: Work\Layout_Temp\PartsDB.pdb

     Number of Part Numbers: 39
          Part Numb: AT24C02C-XHM -> Vend Part: AT24C02C-XHM 
          Part Numb: CRCW040210R0F100 -> Vend Part: CRCW040210R0F100 
          Part Numb: CRCW040216K2FKED -> Vend Part: CRCW040216K2FKED 
          Part Numb: CRCW040249R9F100 -> Vend Part: CRCW040249R9F100 
          Part Numb: CRCW040288K7FKED -> Vend Part: CRCW040288K7FKED 
          Part Numb: CRCW04020000Z0ED(UN) -> Vend Part: CRCW04020000Z0ED(UN) 
          Part Numb: CRCW04021002F100(UN) -> Vend Part: CRCW04021002F100(UN) 
          Part Numb: CRCW04023301F100 -> Vend Part: CRCW04023301F100 
          Part Numb: CR0402-16W-000T -> Vend Part: CR0402-16W-000T 
          Part Numb: C0402C152J5GACTU -> Vend Part: C0402C152J5GACTU 
          Part Numb: C1005X7S1A105K050BC -> Vend Part: C1005X7S1A105K050BC 
          Part Numb: DUT_RUG8 -> Vend Part: DUT_RUG8 
          Part Numb: ERF8-025-01-L-D-RA-L-TR -> Vend Part: ERF8-025-01-L-D-RA-L-TR 
          Part Numb: ERJ-2GEJ105 -> Vend Part: ERJ-2GEJ105 
          Part Numb: ERJ-2GEJ152 -> Vend Part: ERJ-2GEJ152 
          Part Numb: ERJ-2GEJ562 -> Vend Part: ERJ-2GEJ562 
          Part Numb: ERJ-2RKF25R5X -> Vend Part: ERJ-2RKF25R5X 
          Part Numb: ERJ-2RKF1002X -> Vend Part: ERJ-2RKF1002X 
          Part Numb: ERJ-2RKF3012X -> Vend Part: ERJ-2RKF3012X 
          Part Numb: ERJ-2RKF5112X -> Vend Part: ERJ-2RKF5112X 
          Part Numb: GRM21BR60J476ME15L -> Vend Part: GRM21BR60J476ME15L 
          Part Numb: GRM155R60G225ME15D -> Vend Part: GRM155R60G225ME15D 
          Part Numb: GRM155R61A104KA01 -> Vend Part: GRM155R61A104KA01 
          Part Numb: GRM155R71C224KA12 -> Vend Part: GRM155R71C224KA12 
          Part Numb: GRM155R71H103KA88D -> Vend Part: GRM155R71H103KA88D 
          Part Numb: GRM188R60J106ME47D -> Vend Part: GRM188R60J106ME47D 
          Part Numb: GRM1555C1H150FZ01D -> Vend Part: GRM1555C1H150FZ01D 
          Part Numb: HEADER,MALE,2PIN,.100CC(UN) -> Vend Part: HEADER,MALE,2PIN,.100CC(UN) 
          Part Numb: OPA835IDBV -> Vend Part: OPA835IDBV 
          Part Numb: REG71055DDC -> Vend Part: REG71055DDC 
          Part Numb: SMA-J-P-X-ST-EM1 -> Vend Part: SMA-J-P-X-ST-EM1 
          Part Numb: SN74AVCH1T45DBVR -> Vend Part: SN74AVCH1T45DBVR 
          Part Numb: TPS3836K33DBVR -> Vend Part: TPS3836K33DBVR 
          Part Numb: TPS62080DSG -> Vend Part: TPS62080DSG 
          Part Numb: TPS79101DBVREP -> Vend Part: TPS79101DBVREP 
          Part Numb: 5001 -> Vend Part: 5001 
          Part Numb: 103321-2 -> Vend Part: 103321-2 
          Part Numb: 502570-0893 -> Vend Part: 502570-0893 
          Part Numb: 744029001 -> Vend Part: 744029001 

     Number of Part Names: 0

     Number of Part Labels: 0


     Checking for value differences between symbol properties and PartsDB properties

     Checking the validity of the packaging of prepackaged schematic
      symbols.  Only the first error in symbols having the same
      Reference Designator will be reported.

     The packaging of all prepackaged schematic symbols is consistent
      with the Parts DataBase data for the cross mapping of
      symbol pin names to Part Number pin numbers.
      Symbols that were not prepackaged will now be packaged correctly.
      
     No errors in Existing Schematic Packaging.

     The Common DataBase has been read and will be packaged.
     Clustering 156 Symbols:
             156  *****
             150  **************************************************
             100  **************************************************
              50  **************************************************
     Clustering is Complete

     Packager Assignments successfully completed



     51 nets were found containing 248 pins
     92 components were found

     After augmentation of supply pins, there are 50 nets where 0 nets have only one pin.

     Creating a formatted Schematic Netlist (LogFiles\SchematicNetlist.txt)...
     A formatted Schematic Netlist has been created.

     The Logic DataBase has been compiled from the Schematic Design.
      Use Netload to bring the Component Design into sync.

     Logic Data has been successfully Compiled with no errors or warnings.
      Please proceed with your component Design.
                                     NetLoad
                                     -------

                        02:05 PM Tuesday, March 11, 2014
Job Name: D:\PCB Projects\Expedition\Nanopower\EVM\ADS704x_SE_EVM\PCB\ADS704x_SE_EVM.pcb


Version:  02.11.12

     Netloading the Layout.  Unused components will be deleted.

     Unconnected pins will be set to net "(Net0)".

     Schematic reference designator changes will be forward annotated.

     Netload completed successfully with 0 warning(s).
     
     Back Annotating...

  Updating Logic Database...

     Version:  99.00.05

     No changes made to Existing Schematic Packaging.


     There is no symbol data to be back annotated to the schematic source.


     The Logic DataBase has been updated and the Common DataBase has
      automatically been brought into sync with the Logic DataBase.
      Please proceed with your design.

     Finished updating the Logic Database.

     Creating a formatted Schematic Netlist (LogFiles\AfterBakAnnoNetlist.txt)...
     A formatted Schematic Netlist has been created.

     Creating a new netlist text file (LogFiles\KeyinNetList.txt)
      from the Logic Database (Work\Layout_Temp\LogicDB.lgc)...
  A new netlist text file has been generated.



                 Beginning Netload on the Layout Design.
           ---------------------------------------------------
	Assigned net XSIG010153 to a trace which was originally on net XSIG010148.
	Assigned net XSIG010153 to a trace which was originally on net XSIG010148.

Some nets were completely deleted from the Layout Design....
	Deleted net XSIG010148, which has no pins, from the Layout Design.

Forward-Annotation on the Layout Design has been successfully completed.

There were 2 reassignments of nets.
There were 0 traces broken back.
There were 1 nets removed from the Layout Design.