![]() |
![]() |
* ============================================================================ * Copyright (c) Texas Instruments Inc 2005 * * Use of this software is controlled by the terms and conditions found in the * license agreement under which this software has been supplied or provided. * ============================================================================ *
Go to the source code of this file.
Defines | |
| #define | MSP430LIB_SUCCESS 1 |
| Indicates success of an API call. | |
| #define | MSP430LIB_FAILURE 0 |
| Indicates failure of an API call. | |
Enumerations | |
| enum | msp430lib_keycode { MSP430LIB_KEYCODE_POWER = 0x300c, MSP430LIB_KEYCODE_CHANINC = 0x3020, MSP430LIB_KEYCODE_CHANDEC = 0x3021, MSP430LIB_KEYCODE_VOLINC = 0x3010, MSP430LIB_KEYCODE_VOLDEC = 0x3011, MSP430LIB_KEYCODE_OK = 0x300d, MSP430LIB_KEYCODE_MENU = 0x302e, MSP430LIB_KEYCODE_MENUDONE = 0x300f, MSP430LIB_KEYCODE_INFOSELECT = 0x300f, MSP430LIB_KEYCODE_SLEEP = 0x3026, MSP430LIB_KEYCODE_SUBTITLE = 0x30cb, MSP430LIB_KEYCODE_REPEAT = 0x3022, MSP430LIB_KEYCODE_1 = 0x3001, MSP430LIB_KEYCODE_2 = 0x3002, MSP430LIB_KEYCODE_3 = 0x3003, MSP430LIB_KEYCODE_4 = 0x3004, MSP430LIB_KEYCODE_5 = 0x3005, MSP430LIB_KEYCODE_6 = 0x3006, MSP430LIB_KEYCODE_7 = 0x3007, MSP430LIB_KEYCODE_8 = 0x3008, MSP430LIB_KEYCODE_9 = 0x3009, MSP430LIB_KEYCODE_0 = 0x3000, MSP430LIB_KEYCODE_ENTER = 0x2039, MSP430LIB_KEYCODE_INPUT = 0x20ff, MSP430LIB_KEYCODE_REWIND = 0x3172, MSP430LIB_KEYCODE_PLAY = 0x3175, MSP430LIB_KEYCODE_FASTFORWARD = 0x3174, MSP430LIB_KEYCODE_RECORD = 0x3177, MSP430LIB_KEYCODE_STOP = 0x3176, MSP430LIB_KEYCODE_PAUSE = 0x3169 } |
| The IR remote keycodes returned by the MSP430. Requires the DVD function on Philips PM4S set to code 020. More... | |
Functions | |
| int | msp430lib_init (void) |
| Initializes the MSP430 library. Must be called before any API calls. | |
| int | msp430lib_get_rtc (int *year, int *month, int *day, int *hour, int *minute, int *second) |
| Get the current Real Time Clock value from the MSP430. | |
| int | msp430lib_set_rtc (int year, int month, int day, int hour, int minute, int second) |
| Set the current Real Time Clock value on the MSP430. | |
| int | msp430lib_get_ir_key (enum msp430lib_keycode *key) |
| Get a new IR key from the msp430 (if any). | |
| int | msp430lib_exit (void) |
| Deinitalize the MSP430 library. No API calls can be made after this function has been called. | |
|
|
Indicates success of an API call.
|
|
|
Indicates failure of an API call.
|
|
|
|
Initializes the MSP430 library. Must be called before any API calls.
|
|
||||||||||||||||||||||||||||
|
Get the current Real Time Clock value from the MSP430.
|
|
||||||||||||||||||||||||||||
|
Set the current Real Time Clock value on the MSP430.
|
|
|
Get a new IR key from the msp430 (if any).
|
|
|
Deinitalize the MSP430 library. No API calls can be made after this function has been called.
|