How to use these files with Code Composer Studio:

1) First Setup the Code Composer Studio with the appropriate Board type/name, I/O port,
   CPU type and GEL file
2) Start the Code Composer Studio and create a new project by selecting Project-New from
   the menu and then select the location and name of the project on the computer
3) From the menu, select Project-Build Options-Target and then on the Compiler Tab choose
   the appropriate device form the Basic-Target Version
4) From the menu choose Project-Add Files to Project and add the vecs.asm and
   mcbsp_to_vbap.c files. Also include the appropriate link command file (*.cmd) and
   library files (*.lib) from C:\ti according to the target C6000 device used
5) In the mcbsp_to_vbap.c file change the #define CHIP_6xxx 1 to the appropriate
   number according to the TMS320C6000 DSP used. For instance if the TMS320C6711 is
   used change the above line to #define CHIP_6711 1
6) Build the project by selecting Project-Build from the menu
7) Load the program by selecting File-Load Program from the menu
8) Run the program