The following files are included:
1.  ADS8411_C6713_DEMO.pjt
2.  C6713_ADS8402.out
3.  c6713dsk_ADS8411_DEMO.wks
4.  Config.cdb
5.  Config.tcf
6.  cc_setup.ccs
7.  Configcfg.cmd
8.  Configcfg.h
9.  Configcfg.h62
10.  Configcfg.s62
11.   Configcfg_c.c
12.  Custom.lkf
13.  Custom.lkv
14.  dc_conf.h
15.  functions.c
16.  main.c
17.  readme.txt

Directions:
1. Unzip these files into a new directory.  
2. Start Code Composer Studio.  
3. Click on the "File" menu, then click on "Workspace" menu item.
4. Find the directory where these files are stored in.  
5. Select c6713dsk_ADS8411_DEMO.wks, and click "Open"
6. Click on "Project", then click on "Rebuild All"
7. Once the source code is compiled, Click  "File" menu, 
   click "Load Program", find and load "C6713_ADS8411.out."
9. Click "Debug" menu, then click  "Run" menu item.

Assuming a analog input has been applied to the converter channel, the user can observe the digital code in code composer studio's graphical display.