The following files are included:
1.  ads8320.asm
2.  ads8320.cmd
3.  ads8220.mak
4.  c5402vec.asm
5.  regs.h  

Directions:
1. Unzip these files into a new directory.  
2. Start Code Composer Studio.  
3. Click on the "Project" menu, then click on "Open" menu item.
4. Find the directory where these files are stored in.  
5. Select ads8320.mak, and click "Open"
6. Click on "Project", then click on "Rebuild All"
7. Once the source code is compiled, Click  "File" menu 
8. Click "Load Program" menu item and select "ads8320.out" to open.
9. Click "Debug" menu, then click  "Run" menu item.

Assuming a differential analog input has been applied to the converter channels, the user can observe the digital code in code composer studio's graphical display at 0x3000 in data space.