SWRA495L December 2015 – April 2025 CC1310 , CC1350 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R-Q1 , CC2650 , CC2662R-Q1
The CC13xx, CC26xx, CC23xx, and CC27xx family are low-power wireless microcontrollers (MCU) platforms supporting multiple standards (that is, Bluetooth® low energy, IEEE® 802.15.4, and proprietary RF protocols). The document is valid for all CC13xx, CC26xx, CC23xx, and CC27xx family devices, unless otherwise noted. The generic term CC devices is used for simplification. The CC devices have integrated 24MHz (CC13x0 and CC26x0) or 48MHz (CC13x2, CC26x2, CC23xx, CC27xx) and 32.768kHz crystal oscillators TI designed for use with low-cost quartz crystals. The 24MHz and 48MHz oscillator (XOSC-HF for CC13xx and CC26xx; HFXT for CC23xx and CC27xx) generates the reference clock for the RF blocks and the MCU system. RF systems are dependent on accurate clocks for correct operation. A deviation in clock frequency is reflected as a deviation in radio frequency. This deviation can degrade RF performance, violate regulatory requirements, or lead to a nonfunctioning system. In power-down mode, the high-frequency oscillator is typically turned off and a low-frequency oscillator is the system clock. For time-synchronized protocols such as Bluetooth low energy, a tight tolerance on the sleep clock enables longer time in low-power mode and reduced power consumption important in battery-powered applications. For this low-frequency oscillator, typically a 32kHz crystal oscillator (XOSC-LF for CC13xx and CC26xx; LFXT for CC23xx and CC27xx) is used.
The scope of this application report is to discuss the requirements and trade-offs of the crystal oscillators for this CC devices and provide information on how to select an appropriate crystal. This document also presents steps to configure the device to operate with a given crystal. You must configure the CC devices based on the crystal used (that is, adjust the internal capacitor array to match the loading capacitor of the crystal for the XOSC-HF). This application report also discusses some measurement approaches that can be used to characterize certain performance metrics, including crystal oscillator amplitude, and start-up time.
SimpleLink™ and SmartRF™ are trademarks of Texas Instruments.
Bluetooth® is a registered trademark of Bluetooth SIG, Inc.
IEEE® is a registered trademark of Institute of Electrical and Electronics Engineers.
ZigBee® is a registered trademark of ZigBee Alliance.
All trademarks are the property of their respective owners.
This section explains fundamentals of a quartz crystal and the oscillator operations required to understand the trade-offs when selecting a crystal for the CC devices. The complete crystal oscillator circuit includes the loading capacitance, crystal, and the on-chip circuitry.