• Menu
  • Product
  • Email
  • PDF
  • Order now
  • What to Do When Your PLL Does Not Lock

    • SSZTB45 July   2016 LMX8410L , TRF370315 , TRF370317 , TRF370333 , TRF370417 , TRF3705 , TRF3710 , TRF371109 , TRF371125 , TRF371135 , TRF372017 , TRF3722 , TRF37T05

       

  • CONTENTS
  • SEARCH
  • What to Do When Your PLL Does Not Lock
  1.   1
  2.   2
    1.     3
    2.     Step 1: Verify Communication
    3.     Step 2: Establish Lock
    4.     Additional Resources
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
Technical Article

What to Do When Your PLL Does Not Lock

Dean Banerjee

Have you ever been frustrated just trying to get your phase-locked loop (PLL) to lock? Premature assumptions can make the debugging process much longer and more tedious than necessary. By following the processes outlined here for verifying communication and establishing lock, the debugging process can be simplified.

Step 1: Verify Communication

The first step is to verify the PLL’s ability to respond to programming. If the PLL is not locking and you cannot read back from it, try sending software commands that require a minimum amount of hardware commands to work. One possibility is to power the PLL up and down via software (not pin) and look for a predictable current change or bias-voltage-level change on a pin. Many PLLs have a bias level on their input (OSCin) pin that is Vcc/2 when powered up and 0V when powered down.

If the PLL has integrated voltage controlled oscillators (VCOs), look at the low-dropout (LDO) output pin voltages and see if they react to power-down and power-up commands. It might be possible to toggle input/output (I/O) pins such as the MUXout pin on many LMX PLLs. If you can verify communications with these methods, then go ahead and try to achieve lock.

If you cannot verify communication, then look for common culprits such as the following:

  • Crossed programming lines
  • Latch enable (also called chip select bar (CSB)) held too high
  • Too much low-pass filtering on the software inputs
  • Timing issues with the Serial Peripheral Interface bus (SPI)
  • Incorrectly soldered power pins.

Step 2: Establish Lock

Once you have verified communication, the next step is to try to achieve lock with the PLL. These are some of the more common reasons for an unlocked PLL:

  • Misinterpretation of the lock detect pin. If configured incorrectly, the lock detect pin can give an indication that the PLL is unlocked when in fact it is locked. It is good practice to verify this condition by looking at the output on a spectrum analyzer, or by looking at the VCO tuning voltage.
  • Programming issues. Incorrect information sent to the PLL can easily cause it not to lock. Some of the more common programming errors include a VCO programmed to a frequency out of range, incorrect settings for VCO calibration or incorrect timing of the registers.
  • VCO calibration issues. For PLLs with integrated VCOs, the frequency range is typically divided into several different bands. Incorrect programming can cause the VCO to lock to the wrong band. The programming of a particular register typically initiates VCO calibration; therefore, you should confirm that the other software and hardware conditions (especially the input reference) are proper when programming this register so that the calibration works correctly.
  • Issues with the input or feedback path. If the input from the VCO or input reference has an issue due to low power level, low slew rate, poor matching or high harmonics, this can cause the PLL to unlock. Most PLLs have a way to output the actual frequency output of the internal counters and send this to a pin.
  • Open or short to ground in the loop filter. You can typically determine open and short by looking at the tuning voltage, or toggling the phase-detector polarity and looking for a frequency change.
  • PLL loop filter instability. It is typically a symptom of instability if lowering the charge-pump current causes the PLL lock, but just because this technique does not work does not rule out instability. Common causes for loop-filter instability include neglecting to account for VCO input capacitance; using an integrated filter that over-restricts the loop bandwidth; or using the PLL with different settings (charge-pump gain, VCO gain, VCO frequency or phase-detector frequency) than the PLL was originally designed for. Various TI tools can simulate loop-filter instability such as the PLLatinum™ simulator tool.

The debugging process for getting a PLL to lock can be much simpler by following a systematic approach and not making premature assumptions. Figure 1 shows a flowchart that can be used to guide one through this process.

GUID-C0C1DD1F-5574-4EFD-AF16-3C7A8BD55926-low.png Figure 1 PLL Debugging Flowchart

If you would like to learn more about the challenges of unlocked PLLs, check out the Texas Instruments portfolio of phase lock loops.

Additional Resources

  • Get started designing with these tools:
    • Clocks and synthesizers (TICS) programming software.
    • CodeLoader software for design register programming.

IMPORTANT NOTICE AND DISCLAIMER

TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.

These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.

TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.

Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 

Copyright © 2023, Texas Instruments Incorporated

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale