• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Large Duty Cycle Operation On the TPS563211

    • SLUAAE4 May   2021 TPS563211

       

  • CONTENTS
  • SEARCH
  • Large Duty Cycle Operation On the TPS563211
  1.   Trademarks
  2. 1TPS563211 Introduction
  3. 2TPS563211 Control Architecture
    1. 2.1 AECM Control on TPS563211
    2. 2.2 AECM Control Principle
  4. 3Large Duty Cycle Operation in the TPS563211
    1. 3.1 On-Time Extension Function
    2. 3.2 TPS563211 EVM Bench Test
    3. 3.3 Summary for Bench Test Results
  5. 4Summary
  6. 5References
  7. 6Also From TI
  8. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Large Duty Cycle Operation On the TPS563211

Trademarks

All trademarks are the property of their respective owners.

1 TPS563211 Introduction

The TPS563211 is a cost effective and highly flexible synchronous buck converter that provides selectable Eco-mode operation or FCCM (Force Continuous Conduction Mode) operation. Selectable Power-Good indicator or external Soft-Start is also configurable through the MODE pin. Power sequencing is possible by correctly configuring the Enable, Power-Good indicator or external Soft-Start. A wide input voltage range of 4.2 V to 18 V supports a wide variety of common input rails like 12 V and 15 V. It supports up to 3 A continuous output current at output voltages between 0.6 V and 7 V.

The device provides fast transient response with true fixed switching frequency through the use of the Advanced Emulated Current Mode (AECM) control topology. With internal smart loop bandwidth control, the device provides fast transient response over a wide output voltage range without the need for external compensation.

2 TPS563211 Control Architecture

2.1 AECM Control on TPS563211

AECM is a new topology based on a fixed-frequency modulator with emulated current information for the loop control, combing the fixed frequency of PCM control and the fast load-transient response of the D-CAP2 control topology. The key features and benefits of AECM include:

  • True fixed-frequency modulation that can simplify EMI filter design and make it easy to achieve high-frequency modulation such as 2.1 MHz.
  • An emulated ramp-generator circuit with smart loop-bandwidth control that can adjust the DC gain smartly, supporting wide-output and large-duty-cycle applications with good load-transient performance.

Figure 2-1 shows the detailed control block diagram in the TPS563211 design.

GUID-20210427-CA0I-VHMX-G47H-DSNSP1NR15XM-low.gif Figure 2-1 TPS563211 Functional Block Diagram

To improve noise immunity with virtually no ripple on the output voltage, an additional RAMP is added. An included error amplifier makes the output voltage very accurate.

In the control block of the TPS563211 device, the inductor valley current is monitored by measuring the SW node voltage during low-side MOSFET ON-time, which leads a minimum off time requirement for the high-side MOSFET. When the ON timer is expired, the high-side MOSFET is turned off and the low-side MOSFET is turned on. The turning off of the high-side MOSFET causes the SW ringing. When measuring the SW node voltage, a time delay needs to be included to let the internal SW node ringing dissipate. This time delay results in the minimum off time for the high-side MOSFET.

Equation 1. GUID-5F138248-AD19-4B1E-AE59-C77F98454C4C-low.gif

Based on Equation 1, since Toff has a minimum value, it follows that the duty cycle, D, has a maximum value. If the FSW is fixed, a smaller TOFF(min), means a larger duty cycle can be supported. Alternatively, if the TOFF(min) is fixed, a larger duty cycle can be supported with a smaller FSW.

In the TPS563211 device, the minimum off time of low-side MOSFET is 105 ns and the maximum on time is 6 μs which result in a maximum duty cycle of about 98% during normal operation.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale