TPS53679, TPS53659, TPS53622 are Intel™ VR13 Serial VID (SVID)-compliant power supply controllers that have programmable parameters. This guide also applies to proprietary footprint devices TPS53678, TPS53658 TPS53655, as well as TPS53681, even though it is not an Intel power controller. The PMBus interface configures the parameter values which are stored into non-volatile memory (NVM) as new boot-up default values. This guide gives a tutorial on NVM programming, and the tools TI provides for the programming process. This guide applies to all the devices in the TI VR13 controller family.
Intel is a trademark of Intel Corporation.
This guide gives an overview of NVM programming for the following TI VR13 controller devices: TPS53679, TPS53659, TPS53622, TPS53678, TPS53658, TPS53655 and TPS53681. Local TI sales and field applications representatives can provide relevant documentation to these devices. This guide gives a technical overview and step-by-step instructions.
Fusion Digital Power Designer is a graphical user interface (GUI) that configures and monitors Texas Instruments digital power controllers, sequencer monitors, and health monitors. The GUI uses the PMBus protocol to communicate with the device over a serial bus using a proprietary USB adapter.
Use the Fusion Digital Power Designer GUI for engineering development. The GUI gives access to all available user-configurable settings, fault information, and telemetry readings. After you configure the device, you can export the settings to a configuration file. The export options are:
Download the latest version of Fusion Digital Power Designer from this URL: http://www.ti.com/tool/fusion_digital_power_designer
The Fusion Manufacturing Tool is a graphical user interface (GUI) that programs TI digital power controllers in a production environment. Download the latest copy of the Fusion Manufacturing Tool from this URL: http://www.ti.com/tool/fusion_mfr_gui
The Fusion Digital Power Designer software operates in online mode when you have connected a device to the system that hosts the software. The software operates in offline mode when you have not connected a device to the system that hosts the software. The software installer provides a different shortcut for each mode.
File | Description | Extension | Type | Compatilble Software |
---|---|---|---|---|
Fusion project file | Contains configuration data for a single device. Intended for engineering development. | .xml | plain-text XML | Fusion Digital Power Designer |
Fusion system file | Contains configuration data for multiple devices. Can be used in engineering development, and production programming. | .tifsp | plain-text XML | Fusion Digital Power Designer, Fusion Manufacturing Tool |
PMBus programmer script | Simplified programming script (comma separated format) for production environment. | .csv | plain-text comma separated value | Fusion Digital Power Designer and third-party tools |
Both Fusion Digital Power Designer and Fusion Manufacturing Tool GUIs use the TI USB-GPIO adapter to interface between a host computer and controller devices. Use this link to get a TI USB-GPIO adapter: http://www.ti.com/tool/usb-to-gpio.
This section shows how to program NVM with the TI software tools, or with non-TI tools.