All trademarks are the property of their respective owners.
The TMUXRTJ-RRQEVM evaluation module (EVM) and its intended use is described in this user's guide. This board allows for the quick prototyping and DC characterization of TI’s line of TMUX products that use 20-pin QFN packages (RTJ or RRQ).
Always follow TI’s setup and application instructions, including use of all interface components within their recommended electrical rated voltage and power limits. Always use electrical safety precautions to help ensure your personal safety and those working around you. Contact TI's Product Information Center http://support/ti./com for further information.
Save all warnings and instructions for future reference.
The term TI HV EVM refers to an electronic product typically provided as an open framed, unenclosed printed circuit board assembly. It is intended strictly for use in development laboratory environments, solely for qualified professional users having training, expertise and knowledge of electrical safety risks in development and application of high voltage electrical circuits. Any other use or application are strictly prohibited by Texas Instruments. If you are not suitably qualified, you should immediately stop from further use of the HV EVM.
Limitation for safe use:
EVMs are not to be used as all or part of a production unit.
The information in the warning statement is provided for personal protection and the information in the caution statement is provided to protect the equipment from damage. Read each caution and warning statement carefully.
The TMUXRTJ-RRQEVM has the following features:
3 power supply decoupling capacitors from VDD to GND (three 3.3 µF capacitors)
1 protection diode pad from VDD to GND available near power supply (6.9 mm × 5.8 mm)
3 power supply decoupling capacitors from VSS to GND (three 3.3 μF capacitors)
1 protection diode pad from VSS to GND available near power supply (6.9 mm × 5.8 mm)
Terminal block power supply connection
DUT footprint compatible with 20-pin RTJ and RRQ (WQFN) packages
20 length-matched signal inputs corresponding to the 20 pins of the DUT
Selectable connections to VDD, VSS, or GND for each signal input using 2.54 mm shunt
Footprints for pull-up and pull-down resistors for each signal input (two 0603 footprints on each of 20 signals)
Footprints for series resistors for each signal input (two 0805 footprints on each of 20 signals)
Footprints for decoupling capacitors for each input (one 1206 footprint and one 1812 footprint on each of 20 signals)
2 test points for each signal input
Selectable thermal pad connection
Multiple GND test point connections around board
There are 20 headers located around the board with designators J1 through J20. These 3-by-2 headers serve as connections to power planes and to signals of the DUT (U1). Each pin of the DUT has similar header and test point configuration. At four different locations around the board, a legend shows the connections of the pins of the nearby five headers. Figure 5-1 shows a representation of the header associated with pin 1 of U1.
The silkscreen legend represents the connections of the pins of J1. Figure 5-2 shows the pin numbers of this header from this same perspective.
Table 5-1 also shows the connections.
Header Pin Number | Connection |
---|---|
1 | No connection |
2 | VDD |
3 | GND |
4 | U1 |
5 | GND |
6 | VSS |
For all headers J1 through J20, the connections are the same, but are rotated by a multiple of 90° according to their position on the board. A legend is included for each rotation.
There is one 3-by-1 header located near the DUT (J21). Pin 2 of this header is connected to the thermal pad of the DUT. Pin 1 of this header is connected to GND, and pin 3 of this header is connected to VSS.
The connections of J21 are also labeled on the board's silkscreen layer next to the header.
In addition to headers, multiple test points are located around the board. Black test points (TP22 and TP24-TP30) are connected to GND, the red test point (TP21) is connected to VDD, and the green test point (TP23) is connected to VSS. The remaining blue test points (TP1-TP20 and TP101-TP120) are connected along the signal paths of the pins of U1.
The last two digits of the blue test point number represent the pin with which the test point is associated. For example, TP16 and TP116 are both pin 16 of U1.
Table 5-2 also shows the test point connections.
Designator | Connection |
---|---|
TP1 | J1.4 |
TP2 | J2.4 |
TP3 | J3.4 |
TP4 | J4.4 |
TP5 | J5.4 |
TP6 | J6.4 |
TP7 | J7.4 |
TP8 | J8.4 |
TP9 | J9.4 |
TP10 | J10.4 |
TP11 | J11.4 |
TP12 | J12.4 |
TP13 | J13.4 |
TP14 | J14.4 |
TP15 | J15.4 |
TP16 | J16.4 |
TP17 | J17.4 |
TP18 | J18.4 |
TP19 | J19.4 |
TP20 | J20.4 |
TP21 | VDD |
TP22 | GND |
TP23 | VSS |
TP24 | GND |
TP25 | GND |
TP26 | GND |
TP27 | GND |
TP28 | GND |
TP29 | GND |
TP30 | GND |
TP101 | U1.1 |
TP102 | U1.2 |
TP103 | U1.3 |
TP104 | U1.4 |
TP105 | U1.5 |
TP106 | U1.6 |
TP107 | U1.7 |
TP108 | U1.8 |
TP109 | U1.9 |
TP110 | U1.10 |
TP111 | U1.11 |
TP112 | U1.12 |
TP113 | U1.13 |
TP114 | U1.14 |
TP115 | U1.15 |
TP116 | U1.16 |
TP117 | U1.17 |
TP118 | U1.18 |
TP119 | U1.19 |
TP120 | U1. 20 |
Terminal block J25 is the power input for the board. Three power rails (VSS, GND, and VDD) are labeled on the board’s silkscreen layer, indicating the identities of the input pins of the header. Connect the power supply rails at this terminal block to power the board.
The TMUXRTJ-RRQEVM will not have any device connected at footprint U1, and there are not any devices included with the EVM for this footprint. Attach any compatible Texas Instruments 20-pin TMUX device to this location, which will serve as the Device Under Test (DUT). Compatible devices include parts with RTJ or RRQ package names.
By default, the TMUXRTJ-RRQEVM will have 2.54 mm shunts on headers J1 through J20 connected such that the pins of U1 are connected to GND. Remove these shunts from J1 through J20 as necessary if these connections are not desired. Alternatively, the pins of U1 can be shorted to VDD or VSS by connecting between pin 4 of the header and one of the other pins on the header. Figure 5-2 and Table 5-1 include detailed descriptions of the connections on J1 through J20.
As shown in Figure 6-2 and Figure 6-3 as R5 and R6 on the J1 (pin 1 of U1) signal line, the TMUXRTJ-RRQEVM includes 0 Ω series resistors (0805 package) on each signal line.
These can be substituted for different resistors as desired. Additionally, there are pads for pull-up and pull-down resistors to VDD and GND respectively. Add any 0603 resistor to the footprint shown here as R1 to provide pull-up to VDD, and add any 0603 resistor to the footprint shown here as R13 to provide pull-down to GND.
Each signal line also includes two footprints that allow for the user to attach capacitors or other devices with matching footprints. On the top side of the board, shown in Figure 6-2 and Figure 6-3 as C1, a standard 1206 footprint exists between the U1 pin signal and the GND signal. The user can solder a capacitor to this footprint to provide capacitance to the signal line.
Figure 6-4 shows that a standard 1812 footprint exists as C101 on the backside of the board, which also allows a capacitor to be connected between the U1 pin signal and GND. The user can solder a capacitor to this footprint to provide capacitance to the signal line.
The user can select the connection of the thermal pad of U1 by using the three-by-one header located near U1 (J21).
Connecting a shunt between pins 1 and 2 of this header will tie the thermal pad of U1 to GND, while connecting pins 2 and 3 will tie the thermal pad of U1 to VSS. Leave pin 2 of this header unconnected to allow the thermal pad to float, or use an external connection to tie the thermal pad to any other potential.
Figure 7-1 shows the layout of the EVM PCB.
Figure 8-1 and Figure 8-2 are schematic views of the TMUXRTJ-RRQEVM that includes all the parts and connections.
Figure 8-3 and Figure 8-4 are schematic views of the TMUXRTJ-RRQEVM that show only the parts that are included in the EVM and excludes the parts that are DNI.
Designator | Component | Manufacturer | Description | Quantity |
---|---|---|---|---|
C21, C22, C23, C24, C25, C26 | CKG57NX7T2E335M500JH | TDK | CAP, CERM, 3.3 µF, 250 V, ± 20%, X7T, AEC-Q200 Grade 1, 6 × 5 × 5 mm | 6 |
H1, H2, H3, H4 | NY PMS 440 0025 PH | B&F Fastener Supply | Machine Screw, Round, #4-40 × 1/4, Nylon, Philips panhead | 4 |
H5, H6, H7, H8 | 1902C | Keystone | Standoff, Hex, 0.5"L #4-40 Nylon | 4 |
J1, J2, J3, J4, J5, J6, J7, J8, J9, J10, J11, J12, J13, J14, J15, J16, J17, J18, J19, J20 | 61300621121 | Wurth Elektronik | Header, 2.54 mm, 3 × 2, Gold, TH | 20 |
J21 | 61300311121 | Wurth Elektronik | Header, 2.54 mm, 3 × 1, Gold, TH | 1 |
J22 | 2-881545-2 | TE | Default shunt positioning: between pins 1 and 2 of J21 | 1 |
J23, J24, J26, J27, J28, J29, J30, J31, J32, J33, J34, J35, J36, J37, J38, J39, J40, J41, J42, J43 | 2-881545-2 | TE | Default shunt positioning: between pins 3 and 4 of J1-J20 | 20 |
J25 | 691 101 710 003 | Wurth Elektronik | Terminal Block, 5 mm, 3 × 1, Tin, TH | 1 |
LBL1 | THT-14-423-10 | Brady | Thermal Transfer Printable Labels, 0.650" W x 0.200" H - 10,000 per roll | 1 |
R5, R6, R7, R8, R9, R10, R11, R12, R21, R22, R23, R24, R25, R26, R27, R28, R37, R38, R39, R40, R41, R42, R43, R44, R52, R53, R54, R55, R56, R57, R64, R65, R66, R67, R68, R69, R76, R77, R78, R79 | PMR10EZPJ000 | Rohm | RES, 0, 0%, W, AEC-Q200 Grade 0, 0805 | 40 |
TP1, TP2, TP3, TP4, TP5, TP6, TP7, TP8, TP9, TP10, TP11, TP12, TP13, TP14, TP15, TP16, TP17, TP18, TP19, TP20, TP101, TP102, TP103, TP104, TP105, TP106, TP107, TP108, TP109, TP110, TP111, TP112, TP113, TP114, TP115, TP116, TP117, TP118, TP119, TP120 | 5122 | Keystone | Test Point, Compact, Blue, TH | 40 |
TP21 | 5005 | Keystone | Test Point, Compact, Red, TH | 1 |
TP22, TP24, TP25, TP26, TP27, TP28, TP29, TP30 | 5011 | Keystone | Test Point, Multipurpose, Black, TH | 8 |
TP23 | 5126 | Keystone | Test Point, Multipurpose, Green, TH | 1 |
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265 Copyright © 2022, Texas Instruments Incorporated |