ZHCU737A June   2016  – May 2019 TPS3828

 

  1.   修订历史记录

Build HYBRID-WMBUS-PLCSoftware Example Using CCS™

The software project can be built with CCS v9.0.1 (or above). The two project files of HybridWmbusPlcExample_CC1310_LAUNCHXL_tirtos_ccs and tirtos_builds_CC1310_LAUNCHXL_release_ccs need to be opened and the CCS project of HybridWmbusPlcExample_CC1310_LAUNCHXL_tirtos_ccs needs to be built. The screen capture of the CCS projects is shown in Figure 15. Once the compilation is successful, the binary file (HybridWmbusPlcExample_CC1310_LAUNCHXL_tirtos_ccs.out) will be generated under the directory of debug.

Figure 14. Build HYBRID-WMBUS-PLC CCS ProjectTIDC-HYBRID-WMBUS-PLC TIDC-HYBRID-WMBUS-PLC-ccs-project-view.png