ZHCU734A January 2017 – March 2020
Real-time emulation is a special emulation feature that allows windows within CCS to be updated while the MCU is running. This feature not only allows graphs and watch windows to update, but also allows the user to change variables or memory location values and have those changes affect the MCU behavior. This feature is very useful when tuning control law parameters on-the-fly, for example.

button.
button in the Expressions Window and select Continuous Refresh Interval…. The refresh rate can be slowed for the Expressions Window variables by changing the Continuous refresh interval (milliseconds) value. A rate of 1000 ms is usually enough for these exercises. Click on Continuous Refresh buttons (
) for the watch view.