ZHCSH26E March 2017 – May 2021 CC3120MOD
PRODUCTION DATA
When a device restart is required, the user may issue a negative pulse on either the nHIB pin (pin 4) or on the nRESET pin (pin 35), keeping the other pulled high, depending on the configuration of the platform. If the nRESET pin is used, the user must insure the following:
To ensure a proper reset sequence, the user must call the sl_stop function prior to toggling the reset.