TIDUE95A April   2018  – April 2020

 

  1.   Revision History

Block Diagram

The mmWave software development kit (SDK) enables the development of mmWave sensor applications using the AWR6843/1843 SOC and EVM. The SDK provides foundational components that let end users focus on their applications. In addition, the SDK provides several demonstration applications, which serve as a guide for integrating the SDK into end-user mmWave applications. This reference design is a separate package installed in addition to the SDK package, and is the "application" portions of the block diagram.

Figure 1. Software Block DiagramTIDEP-01001 tidep-01001-software-block-diagram.gif