TIDUE71D March   2018  – April 2020

 

  1.   Revision History

Software Block Diagram of People-Counting Application

As shown in Figure 3, the implementation of the people-counting application demo on the IWR6843 consists of a signal chain running on the C674x DSP, and the tracking module running on the ARM®Cortex®-R4F processor.

At its core, the demo does two things:

  1. Use the radar data to produce a point cloud with each point containing an X, Y and Z coordinate, radial velocity, and SNR (signal to noise ratio)
  2. Finds and tracks clusters in the point cloud.
The point cloud generation uses a unique angle of arrival algorithm, called Capon Beamforming, which has only been implemented by TI in this demo. The tracking algorithm used is developed by TI and used in a variety of our applications. The rest of the document will explain how the signal chain and tracker function.

  • Range processing:
    • For each antenna, 1D windowing, and 1D fast Fourier transform (FFT)
    • Range processing is interleaved with the active chirp time of the frame
    • Implemented on HWA and Cortex R4F
  • Capon Beamforming (BF):
    • Static clutter removal
    • Covariance matrix generation, angle spectrum generation, and integration is performed
    • Outputs range-angle heat map
    • Implemented on c674 DSP
  • CFAR detection algorithm:
    • Two-pass, constant false-alarm rate
    • First pass cell averaging smallest of CFAR-CASO in the range domain, confirmed by second pass cell averaging smallest of CFAR-CASO in the angle domain, to find detection points.
    • Implemented on c674 DSP
  • Elevation Beamforming
    • Capon BF algorithm is applied again for each point detected in Range-Azimuth heatmap
    • 1-D Elevation Spectrum is generated and strongest signal is taken as the detected angle
    • Implemented on c674 DSP
  • Doppler estimation:
    • For each detected [range, azimuth] pair from the detection module, estimate the Doppler by filtering the range bin using Capon beam-weights, and then run a peak search over the FFT of the filtered range bin.
    • Implemented on c674 DSP
  • Tracking:
    • Operates on point cloud
    • Searches for clusters in Cartesian + Doppler Space
    • Predicts movement of clusters to maintain a track of unique objects such as people
    • Output of the tracker is a set of trackable objects with certain properties like position, velocity, physical dimensions, and point density
    • Implemented on Cortex R4F
  • Figure 3. People Counting Application Block Diagram TIDEP-01000 caponsoftwareBlockDiagram.jpg