SWRZ101B December   2021  – December 2023 AM2732 , AM2732-Q1

 

  1.   1
  2.   Abstract
  3. 1Silicon Usage Notes and Advisories Matrices
    1.     Devices Supported
  4. 2 Usage Notes and Advisories
    1.     Silicon Usage Notes
      1.      i2293
      2.      i2295
      3.      i2300
      4.      i2324
      5.      i2364
      6.      i2389
      7.      i2390
    2.     Silicon Advisories
      1.      i2162
      2.      i2288
      3.      i2289
      4.      i2294
      5.      i2297
      6.      i2298
      7.      i2299
      8.      i2301
      9.      i2302
      10.      i2309
      11.      i2315
      12.      i2318
      13.      i2329
      14.      i2336
      15.      i2337
      16.      i2338
      17.      i2339
      18.      i2340
      19.      i2341
      20.      i2342
      21.      i2344
      22.      i2345
      23.      i2387
      24.      i2392
      25.      i2394
      26.      i2386
  5.   Trademarks
  6. 3Revision History

i2392

Race condition in mem-init capture registers resulting in events miss

Details:

Potential race condition in capture registers resulting in events getting lost while other events in the same register are being cleared by writing to the register. Following registers are impacted by this issue:

MSS_CTRL ,DSS_CTRL, DSS_HWA_CFG : *MEMINIT_DONE registers

Workaround(s):

Any of the following Workarounds can be used:

Sequentially trigger the mem-init and clear the status before triggering the new mem-init. This is needed if both the status are in the same register.

(OR)

If parallel triggers are must then poll for the all status-bits that got triggered to be 1'b1 and then go and clear the DONE status register

(OR)

Check the MEM_INIT_STATUS register after starting the mem-init and wait the status to go -low by checking it in regular interval and finally clear the DONE status register when the status goes low