SWRZ101B December   2021  – December 2023 AM2732 , AM2732-Q1

 

  1.   1
  2.   Abstract
  3. 1Silicon Usage Notes and Advisories Matrices
    1.     Devices Supported
  4. 2 Usage Notes and Advisories
    1.     Silicon Usage Notes
      1.      i2293
      2.      i2295
      3.      i2300
      4.      i2324
      5.      i2364
      6.      i2389
      7.      i2390
    2.     Silicon Advisories
      1.      i2162
      2.      i2288
      3.      i2289
      4.      i2294
      5.      i2297
      6.      i2298
      7.      i2299
      8.      i2301
      9.      i2302
      10.      i2309
      11.      i2315
      12.      i2318
      13.      i2329
      14.      i2336
      15.      i2337
      16.      i2338
      17.      i2339
      18.      i2340
      19.      i2341
      20.      i2342
      21.      i2344
      22.      i2345
      23.      i2387
      24.      i2392
      25.      i2394
      26.      i2386
  5.   Trademarks
  6. 3Revision History

i2300

ESM: nerror gets asserted in safety-enabled test cases when warm reset is asserted multiple times.

Details

Glitches are observed on some ESM error lines just after warm reset is asserted. These glitches get captured in the ESM status registers as valid errors. After de-asserting warm reset, these errors are still pending, since these registers are cleared on power-on reset. When nerror is unmasked, these errors are seen at the nerror PAD.

Workaround

To avoid this issue, the safety enable sequence should clear all the ESM status registers at the start.