SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Automatic phase transition requires that the setup phase needs less than 17 sample clock periods to charge the S-H capacitor to the target voltage. This is generally not the case when the Reference DAC drives an external load.
Configure the automatic phase control with the sequence as follows:
The transition sets the AUX_EVCTL:EVSTAT3.AUX_DAC_HOLD_ACTIVE event.