SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The timer measures signal period and pulse width of two different signals A and B. In this example, it is assumed that both signals have periods less than the counter range. Hence, time-out detection as described in the register documentation is not required. Configure as follows:
Figure 20-25 shows how the timer counter first synchronizes to signal A. Channel 0 then captures the high phase of signal A into CH0PCC at time t0. Finally, the period of signal A is captured in CH0CC at time t1. At the same time, Channel 0 sets the event output 0 high, and the timer counter starts to synchronize to signal B. Channel 1 then captures the low phase of signal B into CH1PCC at time t2. Finally, the period of signal B is captured in CH1CC at time t3. At the same time, channel 1 sets the event output 1 high, and the timer counter starts to synchronize to signal A. The sequence then repeats itself until it is stopped by the user.