SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The COMPA positive input can connect to:
The reference DAC output connection is not intended for COMPA usage. Hence, the connection shows as dotted in Figure 20-30.
The user must ensure that the positive input of the COMPA peripheral has only one driver at all times. To avoid shorting signals together internally, TI provides ROM-based TI-DriverLib functions that ensure a break-before-make switching of the internal muxes.