SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The CMD_IEEE_MOD_FILT command takes a command structure as defined in Table 26-68.
CMD_IEEE_MOD_FILT must only be sent while an RX operation is running. On reception, the radio CPU modifies the values of frameFiltOpt and frameTypes for the running process into the values given by newFrameFiltOpt and newFrameTypes, respectively. The radio CPU updates the command structure.
The new values of the frame-filtering options are used from the next time frame filtering is started. If autoAckEn or slottedAckEn are changed, the change applies from the next time reception of a packet ends.
If the command is issued without an active or suspended background-level RX operation, the radio CPU returns the result ContextError in CMDSTA. If any of the parameters entered are illegal, the radio CPU returns the result ParError in CMDSTA. Otherwise, the radio CPU returns DONE.