SPRZ570A November   2023  – May 2024 AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
  4. 2Silicon Revision 1.0 Usage Notes and Advisories
    1. 2.1 Silicon Revision 1.0 Usage Notes
      1.      i2324
    2. 2.2 Silicon Revision 1.0 Advisories
      1.      i2189
      2.      i2310
      3.      i2374
      4.      i2311
      5.      i2345
      6.      i2351
      7.      i2352
      8.      i2353
      9.      i2354
      10.      i2356
      11.      i2357
      12.      i2358
      13.      i2359
      14.      i2383
      15.      i2392
      16.      i2393
      17.      i2394
      18.      i2401
      19.      i2403
      20.      i2404
      21.      i2405
      22.      i2426
      23.      i2427
      24.      i2428
      25.      i2433
      26.      i2438
      27.      i2439
  5. 3Trademarks
  6. 4Revision History

i2345

CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks

Details:

Each memory bank in SoC has a separate memory controller. Even though memory addresses are contiguous, each bank is a separate entity with a separate controller.

If a memory bank received a memory request say 32 bytes and address of memory request is 16 bytes before end of memory bank, the behavior of the memory controller will be:

When the memory controller encounters end of memory bank after 16 bytes it will wrap around and give 16 bytes from the start of the memory bank.

This results in the packet corruption.

Workaround(s):

Ensure from application side single ethernet packet does not span across memory banks.