SPRUJF2A March 2026 – March 2026 AM13E23019
The BCR provides mass erase and factory reset functionality through commands sent to the device over SWD from a debug probe using the debug subsystem mailbox (DSSM). When the device is not configured for SWD disabled, the mass erase and factory reset commands can be individually configured to be enabled with a unique 128-bit password, or disabled. By default, both commands are enabled.
The SWD mass erase and factory reset DSSM commands supersede any static write protection policies. For example, if SWD factory reset is configured to be enabled or enabled with password, the BCR configuration data can be reset even if it is statically write protected.
A SWD mass erase is an erase of the MAIN flash regions only, which typically includes the user application. The BCR and BSL policies stored in the NONMAIN flash region are not affected by a mass erase. A mass erase is useful for erasing all application code and data while leaving the device configuration itself intact.
To set the mass erase command mode and password, configure the BOOTCFG3.MASSERASECMDACCESS field and the PWDMASSERASE password fields in the NONMAIN memory.
A SWD factory reset is an erase of the MAIN flash regions followed by a reset of the NONMAIN flash region to default values. Such an erase is useful for completely resetting the BCR and BSL device boot policies while also erasing the application code and data.
To set the factory reset command mode and password, configure the BOOTCFG3.FACTORYRESETCMDACCESS field and the PWDFACTORYRESET password fields in the NONMAIN memory.