SPRUJF2A March 2026 – March 2026 AM13E23019
When setting up the initial IOMUX configuration for an IO after a BOOTRST, application software can select which digital peripheral from the supported options is to be connect to an IO by writing the appropriate peripheral select value to the PF field while simultaneously setting the PC and INENA bits in the PINCMx register corresponding to the targeted pin. The IOMUX configurations for a given peripheral must be set before the peripheral connected to the IOs has been initialized for operation.
To change the peripheral function selection for a digital IO at runtime after a peripheral function has already been configured for that IO, the following procedure must be followed:
At runtime, the INENA bit can be used to mask the input from the IO to the peripheral, if desired. When INENA is cleared, a connected digital peripheral sees a logic low (0) from the IO, regardless of the external state of the IO. If an IO supports wakeup from SHUTDOWN mode, the INENA bit also controls propagation of the IO state to the SHUTDOWN mode wakeup logic.
If a peripheral is assigned to an IO, but the peripheral is in a disabled state, the last valid output conditions (output logic level and Hi-Z state) are latched in the IOMUX output logic. When the peripheral is enabled, the IOMUX releases the latched state to allow the (now enabled) peripheral's output state to propagate to the IO. The PMCU indicates to the IOMUX when a peripheral is entering a disabled state via the IORET signal, which is combined with the PC signal via a logic OR to control the output state latches. This mechanism handles preservation of the last valid output state of peripherals in power domain 1 (PD1) when entering STOP or STANDBY mode, as PD1 peripherals are always temporarily disabled upon entry to STOP/STANDBY, and re-enabled upon exit from STOP/STANDBY modes.
When no peripheral function is selected (PF==0) the output latches are put into a reset state, causing the output NMOS and PMOS to be disabled (leaving the IO pin in a Hi-Z state with the exception of any enabled pullup/pulldown resistors). Note that the pullup/pulldown resistors are never controlled by either a connected peripheral or the peripheral muxing logic. These resistors are only controlled by the IOMUX control bits.