SPRUIM2J May 2020 – May 2026 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
In the unlikely event that channel synchronization is corrupted, a channel may fail to teardown gracefully, even with flush enabled. If this occurs, the channel may be reset by clearing the PDMA_PSILCFG_TX_ENABLE[31] ENABLE bit. This will cause a local reset of the entire channel, including TR and pairing registers. Note that it does not reset the paired-DMA peer. Resetting the paired-DMA peer is also required before re-initializing and re-pairing the channel.