SLVSJM6 November 2025 MSPM0G5115 , MSPM0G5116 , MSPM0G5117 , MSPM0G5187
The package diagrams below indicate the package symbolization scheme, which is the pre-prod version. After device release, RTM version will be added here. Table 5-1 defines the device revision to version ID mapping.
| Revision Letter | Version (in the device factory constants memory) |
|---|---|
B | 1 |
The revision letter indicates the product hardware revision. Advisories in this document are marked as applicable or not applicable for a given device based on the revision letter. This letter maps to an integer stored in the memory of the device, which can be used to look up the revision using application software or a connected debug probe.