SLVSDZ4D February 2018 – February 2020
PRODUCTION DATA.
This application example demonstrates how the TPS2HB35-Q1 device can be used to power resistive heater loads in automotive seats. In this example, we consider dual heater loads that are powered independently by the two channels of the device. A dual-channel device is the ideal solution as it will yield a smaller solution size relative to two single-channel devices.