SLVSDZ4D February 2018 – February 2020
PRODUCTION DATA.
The DC current in each channel under maximum load power condition will be around 3 A. Both heater loads can be ON at the same time, so the case where both channels are enabled simultaneously is considered to assume worst case heating.
Power dissipation in the switch is calculated in Equation 4. RON is assumed to be 75 mΩ because this is the maximum specification at high temperature. In practice, RON will almost always be lower.
If both channels are enabled, then the total power dissipation is 1.35 W. The junction temperature of the device can be calculated using Equation 6 and the RθJA value from the Specifications section.
The maximum junction temperature rating for the TPS2HB35-Q1 device is TJ = 150°C. Based on the above example calculation, the device temperature will stay below the maximum rating.