All trademarks are the property of their respective owners.
Smart meters, including gas and water meters need to record information such as gas or water consumption and then communicate this information to a data center. Wireless communication commonly uses methods such as, NB-IoT, LoRa and ZigBee®. Take NB-IoT as an example, the typical range of input voltage of a NB-IoT module (such as the ZTE ZM8300G module) is from 3 V to 4.2 V, with a typical voltage of 3.6 V (reference 1 ). The current consumption is similar to Figure 1-1. The typical peak current is about 250 mA.
Most smart meters are powered by LiMnO2 (lithium manganese dioxide) or LiSOCl2 batteries and need to support 10 years or more of operation. Because the voltage of a LiSOCl2 battery (about 3.6 V) is higher than a LiMnO2 battery (about 2-3 V), a LiSOCl2 battery can better support a 3-V electromagnetic valve, which why it is a more popular choice for smart meter applications. The weakness of a LiSOCl2 battery is that the maximum continuous current and pulse current capability is limited. Take an 8.5 Ah LiSOCl2 battery (Tadiran TL-4920(ER26500)) as an example, the maximum recommended continuous current is 75 mAand the maximum 1 sec. pulse capability is 200 mA (reference 2). Because of this, it is common to parallel the hybrid layer capacitor (HLC) or the supercapacitor with the LiSOCl2 battery to support the high pulse current for data transmission. Another characteristic of the LiSOCl2 battery is that the battery capacity is related to the discharging current and the working temperature as shown in Figure 1-2 (reference 2). The battery capacity is about 8.5 Ah with 3-mA discharging current at 25 °C, which is shown in the ER26500 data sheet. However, the capacity drops to 2 Ah (a 76% reduction) with a 100 mA load. It is better to control the discharge current of a LiSOCl2 battery to get a higher capacity and thus, increase the working lifetime (reference 3).
The traditional solution is the direct battery connection solution, like Figure 2-1. The communication model such as NB-IoT is connected with the LiSOCl2 and HLC package directly. The voltage of the LiSOCl2 and HLC package is about 3.6 V at room temperature. When the smart meter does the transmission, the HLC supports the high pulse current for the NB-IoT. During sleep mode, the LiSOCl2 charges the HLC and supports the whole system consumption.
The disadvantage of the direct battery connection solution is customers must choose HLC1550 instead of HLC1520. Because the LiSOCl2 and HLC package has the poor performance at cold temperature (-25 degC or -40 degC) , like in Figure 2-2 and Figure 2-3. Figure 2-2 is the performance of ER26500 and HLC1520 at high pulse current (250 mA / 250 ms). In the waveform, the voltage of the battery package is down to 3.4 V at high pulse current. It is too little margin to power the whole system. Figure 2-3 is the performance of ER26500 and HLC1550, because HLC1550 has a bigger size and higher current capability, the voltage is down to 3.6 V, and it can support the whole system and do the transmission. But HLC1550 has bigger size and higher cost.
Another disadvantage of this solution is the discharge current of LiSOCl2 is uncontrolled. In the Figure 2-2 and Figure 2-3, the discharge current of LiSOCl2 is up to 15 mA and 5 mA, respectively. The LiSOCl2 cannot achieve the maximum capacity, referring Figure 1-2.
One of the cost competitive solutions is the pure boost (TPS61094 or TPS610995) solution (reference 4), similar to Figure 2-4. In this solution, customers could use HLC1520(vender: Tadiran), SPC1520(vendor: EVE) or UPC1520(vender: HCB) and they need to add a pure boost (TPS61094 or TPS610995) to regulate output voltage to about 3.6 V over the whole temperature range. This solution is not sensitive to HLC vendor and size, so the total cost is more competitive than the connecting battery directly.
The weakness of the pure boost solution is that the discharge current of LiSOCl2 battery is uncontrolled. We cannot get the maximum LiSOCl2 battery capacity, and the end-off voltage of the battery package is not controllable. If the terminal voltage is too low(< 2 V), it has unrecoverable effects on the battery lifetime.
The TPS61094 could offer a solution exchanging the HLC to a supercap, which can reduce the total solution cost while still controlling the LiSOCl2 battery discharge current to achieve the maximum capacity and working lifetime, as shown in the Figure 3-1.
The TPS61094 is a synchronous bi-directional buck/boost converter with a bypass switch between input and output (reference 5). When the TPS61094 works in buck mode to charge the supercap, the charging current and the charging termination voltage are programmable with two external resistors (R3 and R2). When the TPS61094 works in boost mode, it can boost the supercap and regulate output voltage to the programmed voltage, set by R1.
The TPS61094 has four operation modes: the auto buck or boost mode; the force buck mode; the force bypass mode and the true shutdown mode, set by the EN and MODE pins. Customers can choose the suitable mode based on their application.
The TPS61094 has 60-nA quiescent current in buck mode or boost mode and 4-nA quiescent current in force bypass mode, which could help the system achieve long lifetime.
In the TPS61094 with supercap solution, the MCU doesn’t need to control the TPS61094. TPS61094 can switch between buck charging mode and boost mode automatically. It can boost the supercap to power the high pulse load at data transmission and then charge the supercap during standby mode.
By setting EN = High and MODE = High, the TPS61094 is enabled to work in the auto buck or boost mode. TI suggests to set output target voltage (setting by R1) is 3.3 V (> 3.6 V – 150 mV), which could help TPS61094 enter the buck charging mode automatically; set charging current to 5 mA, which could help get the maximum LiSOCl2 capacity, according to Figure 1-2; set charging terminal voltage to about 2 V, which could help supercap get lower leakage current and longer working life time.
TI suggests to add a series resistor (Rin) of about 40 Ω between LiSOCl2 battery and TPS61094 VIN pin. It could help limit the LiSOCl2 battery discharge current during data transmission. The LiSOCl2 battery discharge current is as
The TPS61094 operation is as shown in the Table 3-1. During stand-by operation in the smart meter, because input voltage is higher than output voltage + 100mV, the TPS61094 enters auto buck mode. The bypass MOS turns on and NB-IoT is powered by LiSOCl2. TPS61094 charges the supercap until it is fully charged. When the NB-IoT does the Rx / Tx transmission, there is a high pulse current at the output of TPS61094, because LiSOCl2 can’t support high pulse current, the input voltage will drop. When TPS61094 detects the input voltage is lower than output voltage + 100mV, the boost mode actives automatically. So the supercap mainly supports the high load current.
System operation | Condition | TPS61094 operation |
---|---|---|
Stand-by; low-current consumption | Vin > Vout_target + 100mV |
Active buck charging mode; charge supercap and keep it fully charged; Bypass MOS turns on; Vout connects with Vin; NB-IoT is powered by LiSOCl2. |
Doing Rx / Tx transmission |
Vin >= Vout_target Vout = Vout_target |
Active boost mode; at high-pulse load, supercap mainly supports the load. |
There is a summary of these three power solutions in Table 4-1. TPS61094 could provide a cost competitive and long lifetime solution in the smart meter. This solution can help smart meter customers exchange hybrid layer capacitor (HLC) to supercap, which could have lower total solution cost.
The TPS61094 with the supercap solution can support 18.4 years and increase operation time by 20% than the pure boost solution. And because the TPS61094 shares the same inductor and input/output capacitors in the supercap charging and discharging, the TPS61094 reduces component count by 50%.
Solution | Lifetime estimation (years) | Advantage | Disadvantage |
---|---|---|---|
The direct battery connection solution | 18.1 | Simple design | Big size HLC1550 (Tadiran) |
The pure boost(TPS61094 or TPS610995) solution | 14.9 | Smaller size HLC and no sensitivity to the vendor, like SPC1520 |
Cannot get the maximum LiSOCl2 capacity because LiSOCl2 discharge current is uncontrollable LiSOCl2 discharge end-off voltage is uncontrolled; it may have unrecoverable effects on the battery lifetime |
The TPS61094 with the supercap solution | 18.4 |
Cost competitive with the supercap Control LiSOCl2 discharge current and end-off voltage Automatically transition; No need for MCU control |
The supercap has leakage current, need to use lower terminal voltage, like 2 V |
Note:
The smart meter lifetime estimation is based on the following conditions:The supercap lifetime is related to the operating temperature and operating voltage. The classical aging model for supercapacitors is Eyring's law that estimates the aging rate, as the Equation 2. This law stipulates that a 200-mV voltage surplus increases the aging by a factor of 2 and have the same effect as a temperature increase of 10 °C. (reference 6, 7, 8)
where
tref Reference lifetime (hours)
Vref Reference applied bias voltage (V)
Tref Reference aging temperature (K)
The smart meter customer can lower the operation voltage according to their life time and operation temperature requirement. There is the estimation lifetime from VINA Tech 3.0V series supercap, as shown in Table 5-1
Temp Voltage (V) |
25 °C Year |
30 °C Year |
40 °C Year |
50 °C Year |
60 °C Year |
70 °C Year |
75 °C Year |
80 °C Year |
---|---|---|---|---|---|---|---|---|
2.1 | 180.5 | 127.7 | 63.8 | 31.9 | 16.0 | 8.0 | 5.6 | 4.0 |
2.2 | 127.7 | 90.3 | 45.1 | 22.6 | 11.3 | 5.6 | 4.0 | 2.8 |
2.3 | 90.3 | 63.8 | 31.9 | 16.0 | 8.0 | 4.0 | 2.8 | 2.0 |
2.4 | 63.8 | 45.1 | 22.6 | 11.3 | 5.6 | 2.8 | 2.0 | 1.4 |
2.5 | 45.1 | 31.9 | 16.0 | 8.0 | 4.0 | 2.0 | 1.4 | 1.0 |
2.6 | 31.9 | 22.6 | 11.3 | 5.6 | 2.8 | 1.4 | 1.0 | 0.7 |
2.7 | 22.6 | 16.0 | 8.0 | 4.0 | 2.0 | 1.0 | 0.7 | 0.5 |
2.8 | 16.0 | 11.3 | 5.6 | 2.8 | 1.4 | 0.7 | 0.5 | 0.4 |
2.9 | 11.3 | 8.0 | 4.0 | 2.0 | 1.0 | 0.5 | 0.4 | 0.3 |
3.0 | 8.0 | 5.6 | 2.8 | 1.4 | 0.7 | 0.4 | 0.3 | 0.2 |
Note: 30% capacitance degradation is considered as the end of life (reference 9).
The supercap leakage current is an important part of performance in the smart meter, which is related to the operating life time. The leakage current depends on temperature, working voltage, capacitance and other parameters (similar to charge duration and short-term history) (reference 10).
For the leakage current, when the supercap working voltage decreases, the leakage current could also decrease, similar to Figure 5-1. For example, the supercap works at 1.8 V, the leakage is about 8 uA (18 % of data sheet spec) at 25 ℃.
The supercap leakage current is related to working temperature, too. The supercap leakage current at 65 ℃ is about 3~4 times as the 25 ℃, in the Figure 5-1.
Note: the test data is based on WEC3R0156QG (3 V 15F) (reference 9).
Because the supercap lifetime and leakage current are strongly related to working voltage, TI suggests to set supercap charging terminal voltage to 2 V, which could achieve 20 years life time at 65 ℃ and the leakage current is about 18% of the datasheet spec.
The capacity of the supercap depends on Rx/Tx transmission loss. Let's take NB-IoT as the example. Assume the transmission internal is 24 h that is once data exchange every day, 3.3 V supply voltage, and a payload of 200 Bytes. The power consumption of one transmission is about 4 J. To leave 20 % margin, the target storage energy is set as 4.8 J (reference 11 and 12). The TPS61094 could support the supercap operation until supercap voltage is down to 0.7 V. So the supercap will discharge from 2 V to 0.7 V, the total discharge power is
The supercap discharge power should be higher than the total loss of NB-IoT transmission, 4.8 J, so smart meter could choose 3 F supercap.
The TPS61094 with supercap solution test waveform overview is as shown in the Figure 6-1. There are three phases in this solution. Phase 1 is the NB-IoT data transmission. The load current is about 250 mA for 250 ms. The TPS61094 could regulate output voltage to 3.3 V and control the battery current within 5 mA. In the phase 2, the NB-IoT stops doing the data transmission, so TPS61094 charges the supercap in setting current about 2.5 mA. As shown in the Figure 6-1, the supercap voltage increases and triggers charging terminal voltage (2 V). The TPS61094 stops charging and this is phases 3. The whole system enters the standby mode and waits for the next NB-IoT transmission.
Note:
The dark blue signal (Channel 1) is TPS61094 output voltage, The purple signal(Channel 1) is LiSOCl2 battery output current, The green signal(Channel 4) is the supercap voltage, The light blue signal(Channel 2) is load current.
The NB-IoT data transmission (phase 1) zoom in waveform is as shown in the Figure 6-2 and Figure 6-3. It can be seen that during high pulse current load emulating NB-IoT module, the output voltage of TPS61094 is regulated at 3.3 V to maintain normal work of system. At the same time, the output current of LiSOCl2 battery is about 5 mA or 6 mA both at -25 degC and 25 degC, so that the LiSOCl2 battery lifetime can be maximized referring Figure 1-2.
Figure 6-4 shows the performance of the supercap from charging to full charge (phase 2 to phase3). During supercap charging phase, the TPS61094 can control the charging current to the set current. Because the resistor Rin(between LiSOCl2 battery and TPS61094 VIN pin), there is about 55 mV voltage drop in the TPS61094 output. When the supercap voltage reaches the set terminal voltage, the TPS61094 stops charging.
The Figure 6-5 is the 3.3-V Vout efficiency graph in boost operation. The efficiency is about 93 % at Vin=2 V Vout=3.3 V Iout=250mA.
The Figure 6-6 is the 3.6-V Vin efficiency graph in buck operation. The efficiency is about 88 % at Vin=3.6 V VCHG=2 V ICHG=2.5 mA.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS. |
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources. |
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products. |
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2021, Texas Instruments Incorporated |