SLUUCN4A January 2023 – February 2024
The Black Box Recorder maintains the last three updates of SafetyStatus() in memory. When entering PERMANENT FAIL mode, this information is written to data flash together with the first three updates of PFStatus() after the PF event.
This information is useful in failure analysis, and can provide a full recording of the events and conditions leading up to the permanent failure.
If there were less than three safety events before PF, then some information will be left blank.