SLUUCN4A January 2023 – February 2024
This command returns the effective impedance based on the pack's ability to provide currents in the time frame of milliseconds. The value for Rhf of all cells is combined and added to any other non-cell pack resistance, such as Pack Resistance and System Resistance. Used in conjunction with TurboVload(), this helps to determine which trigger voltage threshold to use so that the system does not fall below its dropout voltage.
SBS Cmd | Name | Access | Protocol | Type | Min | Max | Default | Unit | ||
---|---|---|---|---|---|---|---|---|---|---|
SE | US | FA | ||||||||
0x68 | TurboRhfEffective() | R | R | R | Word | I2 | 0 | 32767 | — | mΩ |