SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
The BCR provides mass erase and factory reset functionality through commands sent to the device over SWD from a debug probe using the debug subsystem mailbox (DSSM). These commands are not available in SWD security level 2, but they are optionally available in security level 0 and 1. When the device is not configured for SWD security level 2, the factory reset can be individually configured to be enabled, enabled with a unique 128-bit password, or disabled. By default, both commands are enabled.
The SWD factory reset DSSM superseded any static write protection policies. For example, if SWD factory reset is configured to be enabled or enabled, the BCR configuration data can be reset even if it is statically write protected.
SWD Factory Reset
A SWD factory reset is an erase of the MAIN flash regions followed by a reset of the NONMAIN flash region to default values. Such an erase is useful for completely resetting the BCR and BSL device boot policies while also erasing the application code and data.
To set the factory reset command mode, configure the BOOTCFG3.FACTORYRESETCMDACCESS field in the NONMAIN memory.