SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
The AES module provides a trigger source which can be configured to source DMA trigger 1. The DMA1 trigger events from the AES are given in Table 33-272. When the DMA1 channel is needed by the AES for block cipher operations, the DMA1 trigger should be unmasked in the IMASK register of DMA_TRIG_DATAOUT and the DMA should be configured as needed to support the AES operation.
| Index (IIDX) | Name | Description |
|---|---|---|
| 0 | NO_INTR | No DMA Trig1 Event Pending |
| 1 | TRIG1 | DMA Trigger for Data Output |
The DMA trigger 1 event configuration is managed with the DMA_TRIG_DATAOUT event management registers. See Using Event Registers for guidance on configuring the event registers for DMA triggers.