SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
To enable multiple-controller mode of operation, the CR.MCTL bit can be set. During the arbitration procedure, the clocks from each different controller must be synchronized. A device that first generates a low period on SCL overrules the other devices, which forces the other devices each to start low periods as well. SCL is then held low by the device with the longest low period. The other devices must wait until the SCL is released before starting high periods.