SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
The code region contains the flash memory used to store executable code and data. Accesses to the flash memory from the CPU through the code region are processed through the AHB bus matrix to the flash read interface directly. The flash memory is aliased to two address spaces in the code region: one in secure address map and the other in non-secure address map.
The code region also contains the read-only memory (ROM) used for the TI device boot code and the bootstrap loader. The ROM is only available during the initial device boot process.