SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
For received data, the data byte and the 4-bit status (break, frame, parity, and overrun) is pushed onto the 12-bit wide receive buffer/FIFO. The error and status can be can be retrieved by reading RXDATA register as showing in Table 22-2. Each of the four below conditions can also set the interrupt flag RXINT if the corresponding interrupt bit is enabled in the IMASK register.
| Error Condition(1) | Bit Field | Description |
|---|---|---|
| Framing error | FRMERR | A framing error occurs when a low stop bit is detected. When two stop bits are used, both stop bits are checked for a framing error. When a framing error is detected, the FRMERR bit is set. |
| Parity error | PARERR | A parity error is a mismatch between the number of 1s in a character and the value of the parity bit. Address bits are included in the parity calculation if included in the character. When a parity error is detected, the PARERR bit is set. |
| Receive overrun | OVRERR | An overrun error occurs when a character is loaded into RXDATA/FIFO before the prior character has been read. When an overrun occurs, the OVRERR bit is set. |
| Break condition | BRKERR | A break is detected when the receive input is held low for longer than a full character transmission time, meaning the start bit, all received data, parity bit, and stop bit/bits are 0. When a break condition is detected, the BRKERR bit is set. |
The UART module flag status can also be checked by reading the STAT register, as shown in Table 22-3.
| Bit Field | Description |
|---|---|
| BUSY | This bit is set as soon as the transmit FIFO becomes non-empty (regardless of whether UART is enabled). In IDLELINE mode (when the CTL0.MODE field is configured for IDLELINE), the BUSY signal also stays set during the idle time generation. |
| RXFE | This bit is set when the receive FIFO is empty. If the FIFO is disabled (FEN is 0), the receive holding register is full. If the FIFO is enabled (FEN is 1), the receive FIFO is full. |
| RXFF | This bit is set when the receive FIFO is full. If the FIFO is disabled (FEN is 0), the receive holding register is empty. If the FIFO is enabled (FEN is 1), the receive FIFO is empty. |
| TXFE | This bit is set when transmit FIFO is empty. If the FIFO is disabled (FEN is 0), the transmit holding register is full. If the FIFO is enabled (FEN is 1), the transmit FIFO is full. |
| TXFF | This bit is set when transmit FIFO is full. If the FIFO is disabled (FEN is 0), the transmit holding register is empty. If the FIFO is enabled (FEN is 1), the transmit FIFO is empty. |
| CTS | This bit is set when CTS signal is asserted (low) and cleared when CTS signal is not asserted (high). |
| IDLE | This bit is set when an IDLE line has been detected in idle-line multiprocessor mode. The IDLE bit is used as an address tag for each block of characters. In idle line multiprocessor format, this bit is set when a received character is an address. |