SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
The AESADV module provides a trigger source which can be configured to source DMA trigger 0. The DMA0 trigger events from the AES are given in Table 33-272. When the DMA0 channel is needed by the AES for block cipher operations, the DMA0 trigger should be unmasked in the IMASK register of DMA_TRIG_DATAIN and the DMA should be configured as needed to support the AES operation.
| Index (IIDX) | Name | Description |
|---|---|---|
| 0 | NO_INTR | No DMA Trig0 event pending |
| 1 | TRIG0 | DMA Trigger for Data Input |
The DMA trigger 0 event configuration is managed with the DMA_TRIG_DATAIN event management registers. See Using Event Registers for guidance on configuring the event registers for DMA triggers.