SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
When multiple HMAC operations need to be performed, using the same MACK keys, but the operation can be interrupted by other hash operations, the performance of the hash operation depends on how fast the MAC keys can be hashed. To increase overall performance the SHA peripheral provides the capability of reading out the inner and outer digest which can be re-loaded for the next operation as shown in Figure 14-5.