SLAU962A December 2025 – June 2026 MSPM33C321A , MSPM33C321A-Q1
The VBOOST circuit in the PMU generates an internal VBOOST supply that is used by the analog muxes in specific modules. The VBOOST circuit enables consistent analog mux performance across the external supply voltage (VDD) range.
Modules supported by VBOOST
Enabling and Disabling VBOOST
SYSCTL automatically manages the enable request for the VBOOST circuit based on the following parameters:
VBOOST is disabled by default following a SYSRST. Application software is not required to enable the VBOOST circuit prior to using associated peripherals. When the peripheral is enabled by application software, SYSCTL also enables the VBOOST circuit to support the peripheral.
The VBOOST circuit has a startup time requirement to transition from a disabled state to an enabled state. If a peripheral is enabled when VBOOST is disabled, then the corresponding peripheral ready status is not asserted until both the peripheral and the VBOOST circuit are ready. If the startup time of the peripheral is less than the VBOOST startup time, the peripheral startup time is then equivalent to the VBOOST startup time.
Alternatively, application software can force the VBOOST circuit to be enabled at all times (with ANACPUMPCFG=0x2) or while in RUN or SLEEP mode (with ANACPUMPCFG=0x1) so that there is no additional startup delay when enabling a peripheral supported by VBOOST. Table 2-1 gives the behavior of the ANACPUMPCFG control and corresponding application use cases.
| VBOOST Control (ANACPUMPCFG) | Behavior | ||
|---|---|---|---|
| VAL | MODE | VBOOST Enable | Application Use Case |
| 0x0 | ONDEMAND | VBOOST is automatically enabled by SYSCTL only when a supported peripheral is enabled. | This setting provides the lowest power consumption in all modes when fast startup of the peripheral is not critical. |
| 0x1 | ONACTIVE | VBOOST is forced to be enabled when the device is in RUN or SLEEP mode. VBOOST is also kept enabled in STOP or STANDBY mode if a supported peripheral is enabled. | This setting provides low power consumption by disabling the VBOOST automatically in STOP and STANDBY modes when no peripherals requiring VBOOST are enabled. VBOOST is automatically re-enabled upon exit to RUN mode to provide fast startup of the supported peripherals in the event that application software enables a said peripheral in RUN mode. |
| 0x2 | ONALWAYS | VBOOST is forced to be enabled in all operating modes except SHUTDOWN. | This setting makes sure that the peripherals never incur additional startup latency due to VBOOST startup in applications where fast startup is critical. |
The VBOOST enable, VBOOST clock selection, and VBOOST clock error logic is shown in Figure 2-4.
VBOOST Clock
The VBOOST circuit requires a functional clock to operate. VBOOST is clocked by either the SYSOSC (4MHz output) or the LFCLK (32kHz) based on the currently active ULPCLK tree source. The VBOOST clock is selected automatically by SYSCTL according to the logic shown in VBOOST Request Logic and described here:
Certain VBOOST operating conditions require that the VBOOST clock be 4MHz (sourced from SYSOSC) and not 32kHz (sourced from LFCLK) for well-designed startup time. Such conditions include:
SYSCTL does not change the current system clock configuration for a VBOOST request. If the ULPCLK tree is sourced from LFCLK in one of these scenarios, SYSCTL asserts an ANACLKERR status in the SYSSTATUS register in SYSCTL to indicate to application software that there is a mismatch between the VBOOST clock requirement and the current ULPCLK configuration.
The complete clock requirements for VBOOST are given in Table 2-2.
| VBOOST Request | VBOOST Circuit Clock Requirement | ULPCLK Source Requirement(1) | Supported Operating Modes or Policies | |
|---|---|---|---|---|
| No active request (VBOOST is disabled) | N/A | Don't care | Don't care | |
| VBOOST is starting up from a disabled state | 4MHz | Not LFCLK | RUN, SLEEP, STOP | |
| COMP enabled | Fast mode (FAST) | 4MHz | Not LFCLK | RUN, SLEEP, STOP |
| Ultra-low-power mode (ULP)(2) | 4MHz or 32kHz | Don't care | RUN, SLEEP, STOP, STANDBY0 | |
| VBOOST running with no peripheral request active (due to ANACPUMPCFG!=0x0)(2) | 4MHz or 32kHz | Don't care | RUN, SLEEP, STOP, STANDBY0 | |
| HFXT | 4MHz or 32kHz | Don't care | RUN, SLEEP, STOP(3) | |