SLAU358Q September 2011 – October 2019
| This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:
(1) this device may not cause harmful interference and (2) this device must accept any interference received, including interference that may cause undesired operation. |
||
| NOTE: This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. However there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:
* Reorient or relocate the receiving antenna * Increase the separation between equipment and receiver * Connect the equipment into an outlet on a circuit different from that to which receiver is connected * Consult the dealer or an experienced radio/TV technician for help. Warning: Changes or modifications not expressly approved by Texas Instruments Inc. could void the user’s authority to operate the equipment. |