SFFSAZ1 January   2026 TLV9161-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
    1. 2.1 SOT-23 (DBV) – 5 Package
    2. 2.2 SOT-SC70 (DCK) – 5 Package
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 SOT-23 (DBV) – 5 Package
    2. 4.2 SOT-SC70 (DCK) – 5 Package
  7. 5Revision History

SOT-SC70 (DCK) – 5 Package

Figure 4-2 shows the TLV9161-Q1 pin diagram for the SOT-SC70 (DCK) – 5 package. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TLV9161-Q1 datasheet.

TLV9161-Q1 Pin Diagram (SOT-SC70 (DCK) –
                                5 Package) Figure 4-2 Pin Diagram (SOT-SC70 (DCK) – 5 Package)
Table 4-6 Pin FMA for Device Pins Short-Circuited to Ground
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
IN+1Device common-mode is tied to the negative rail. Depending on the circuit configuration, the output does not respond because the device is in an invalid, common-mode condition.C
IN‒3The device does not receive negative feedback. Depending on the circuit configuration, the output moves to the negative supply.B
OUT4Depending on the circuit configuration, the device is forced into a short-circuit condition with the OUT voltage ultimately forced to the V‒ voltage. Prolonged exposure to short-circuit conditions can result in long-term reliability issues.A
V+5Op amp supplies are shorted together, leaving the V+ pin at some voltage between the V+ and V‒ sources (depending on the source impedance).A
Table 4-7 Pin FMA for Device Pins Open-Circuited
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
IN+1Device common-mode is disconnected. The op amp is not provided with common-mode bias, and the device output results at the positive or negative rail. The IN+ pin voltage results at the positive or negative rail because of leakages on the ESD diodes.B
V‒2The negative supply remains floating. The op amp ceases to function because no current can source or sink to the device.B
IN‒3The inverting pin of the op amp is left floating. Negative feedback is not provided to the device, resulting in the device output moving between the positive and negative rails. The IN‒ pin voltage ends up at the positive or negative rail because of leakages on the ESD diodes.B
OUT4There is no negative feedback or ability for OUT to drive the application.B
V+5The positive supply is left floating. The op amp ceases to function because no current sources or sinks to the device.A
Table 4-8 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin NamePin No.Shorted toDescription of Potential Failure EffectsFailure Effect Class
IN+1V‒Device common-mode is tied to the negative rail. Depending on the circuit configuration, the output does not respond because the device is in an invalid common-mode condition.C
V‒2IN‒The device does not receive negative feedback. Depending on the circuit configuration, the output moves to the negative supply.B
IN‒3OUTDepending on the circuit configuration, the circuit gain is reduced to unity gain, and the application cannot function as intended.B
OUT4V+Depending on the circuit configuration, the device is likely to be forced into a short-circuit condition with the OUT voltage ultimately forced to the V+ voltage. Prolonged exposure to short-circuit conditions can result in long-term reliability issues.A
V+5IN+Depending on the circuit configuration, the application likely does not function because device common-mode voltage is connected to V+.B
Table 4-9 Pin FMA for Device Pins Short-Circuited to Supply
Pin NamePin No.Description of Potential Failure EffectsFailure Effect Class
IN+1Depending on the circuit configuration, the application does not function because device common-mode voltage is connected to IN+.B
V‒2Op amp supplies are shorted together, leaving the V‒ pin at a voltage amount between the V‒ and V+ sources (depending on the source impedance).A
IN‒3The device does not receive negative feedback. Depending on the noninverting input voltage and circuit configuration, the output can move to the negative supply.B
OUT4Depending on the circuit configuration, the device is forced into a short-circuit condition with the OUT voltage forced to the V+ voltage. Prolonged exposure to short-circuit conditions can result in long-term reliability issues.A