SFFS340A February   2022  – December 2025 LM5164

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
  7. 5Revision History

Pin Failure Mode Analysis (Pin FMA)

This section provides a failure mode analysis (FMA) for the pins of the LM5164. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
ClassFailure Effects
APotential device damage that affects functionality.
BNo device damage, but loss of functionality.
CNo device damage, but performance degradation.
DNo device damage, no impact to functionality or performance.

Figure 4-1 shows the LM5164 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the LM5164 datasheet.

LM5164 Pin Diagram Figure 4-1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • The application circuit is configured per the LM5164 datasheet.
    • The PGOOD pin is pulled up to VOUT.
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No Description of Potential Failure Effects Failure Effect Class
GND 1 N/A D
VIN 2 VOUT = 0V. B
EN/UVLO 3 VOUT = 0V. B
RON 4 VOUT is unregulated; 0 ≤ VOUT < set voltage. B
FB 5 VOUT > set voltage. The PGOOD pin can become damaged if VIN > 14V. A
PGOOD 6 The flag of the PGOOD pin is invalid. B
BST 7 VOUT = 0V. B
SW 8 The power FET is damaged. A
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No Description of Potential Failure Effects Failure Effect Class
GND 1 VOUT = 0V. B
VIN 2 VOUT = 0V. B
EN/UVLO 3 VOUT = 0V. B
RON 4 VOUT > set voltage. B
FB 5 VOUT > set voltage. The PGOOD pin can become damaged if VIN > 14V. A
PGOOD 6 The flag of the PGOOD pin is invalid. B
BST 7 VOUT = 0V. B
SW 8 VOUT = 0V. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No Short to Description of Potential Failure Effects Failure Effect Class
GND 1 VIN The input is grounded. The device is disabled. VOUT = 0V. B
VIN 2 EN/UVLO There is no impact on functionality. D
EN/UVLO 3 RON The device is potentially disabled. B
The device potentially operates at an incorrect frequency if the EN pin is connected to the VIN pin through a resistor, depending on the resulting voltage of the EN pin from the specific resistor network. C
The device is potentially damaged if the EN pin is directly shorted to the VIN pin. A
RON 4 N/A N/A D
FB 5 PGOOD There is no impact on functionality if there is no external pullup at the PGOOD pin. D
VOUT is potentially lower than the set-point if an external pullup exists at the PGOOD pin. C
PGOOD 6 BST The device cannot start up due to the pulldown of the PGOOD pin, which prevents the BST voltage from being established. VOUT = 0V. B
When the short occurs during operation, the PGOOD pin is potentially damaged if the absolute maximum voltage rating of the PGOOD pin is exceeded. A
BST 7 SW Boot voltage cannot be established, and the device is disabled. VOUT = 0V. B
VOUT potentially equals the internal VDD (5V) minus the diode drop of the internal boot diode if the output rail is an open circuit. B
VOUT potentially drops to 0V if the load exceeds the internal VDD of the current limit of the LDO. VOUT = 0V. B
SW 8 N/A N/A D
Table 4-5 Pin FMA for Device Pins Short-Circuited to Supply
Pin Name Pin No Description of Potential Failure Effects Failure Effect Class
GND 1 VOUT = 0V. B
VIN 2 N/A D
EN/UVLO 3 N/A D
RON 4 VIN > 5.5V can lead to device damage. A
FB 5 VIN > 5.5V can lead to device damage. A
PGOOD 6 VIN > 14V can lead to device damage. A
BST 7 VOUT = 0 V. B
SW 8 VOUT = VIN. The PGOOD pin can be damaged if VIN > 14V. A