SFFS310A April   2022  – May 2022 TPS3704 , TPS3704-Q1

 

  1.   Trademarks
  2. 1Purpose of the Functional Safety Report
  3. 2Summary of Assessment
  4. 3Product Description
  5. 4Fulfillment of IEC 61508:2010 Requirements
  6. 5Fulfillment of ISO 26262:2018 Requirements
  7. 6Revision History

Fulfillment of IEC 61508:2010 Requirements

Texas Instruments carried out this assessment with respect to relevant requirements from the IEC 61508:2010 standard.

Table 4-1 Details of IEC 61508:2010 Requirements
IEC 61508:2010 Requirement Status Compliance Argument Evidence
Part 1: General Requirements a. Documentation Pass All documentation follows TI Functional Safety Hardware development flow requirements. All documentation is planned in the functional safety plan. All documentation is following the TI functional safety templates. TI Functional Safety Hardware development flow
Part 1: General Requirements b. Management of Functional Safety Pass Project manager and Safety manager were appointed to this project. Functional Safety Plan was generated and necessary audits and assessments were scheduled. Documented nomination of Functional Safety Manager
Part 1: General Requirements c. Safety Lifecycle - Concept Pass Functional safety concept for the IC was developed with respect to the context of the targeted functional safety systems. System Functional Safety Assumptions and Component Safety Requirements
Part 1: General Requirements d. Safety Lifecycle - Overall Scope Definition N/A Requirements do not apply, however assumptions were made for the SEooC development. N/A
Part 1: General Requirements e. Safety Lifecycle - Hazard and Risk Analysis N/A Requirements do not apply, however assumptions were made for the SEooC development. N/A
Part 1: General Requirements f. Safety Lifecycle - Overall Safety Requirements N/A Requirements do not apply, however assumptions were made for the SEooC development. N/A
Part 1: General Requirements g. Safety Lifecycle - Overall Safety Requirements Allocation Pass Functional safety concept for the IC was developed with respect to the context of the targeted functional safety systems. System Functional Safety Assumptions and Component Safety Requirements
Part 1: General Requirements h. Safety Lifecycle - Overall Operation and Maintenance Planning N/A The requirements for overall operation and maintenance planning do not apply to this SEooC development. N/A
Part 1: General Requirements i. Safety Lifecycle - Overall Safety Validation Planning Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements were planned to be validated in pre-silicon and post-silicon testing. Validation and Characterization Plans
Part 1: General Requirements j. Safety Lifecycle - Overall Installation and Commissioning N/A The requirements for overall installation and commissioning do not apply to this SEooC development. N/A
Part 1: General Requirements k. Safety Lifecycle - E/E/PE System Safety Requirements Specification Pass Functional safety concept for the IC was developed with respect to the context of the targeted functional safety systems. Functional Safety Requirements Specification (SRS)
Part 1: General Requirements l. Safety Lifecycle - E/E/PE Safety-Related Systems: Realization Pass IC functional safety requirements were realized in the product design. Design Specification
Part 1: General Requirements m. Safety Lifecycle - Other Risk Reduction Measures: Specification and Realization N/A The requirements for other risk reduction measures do not apply to this SEooC development. N/A
Part 1: General Requirements n. Safety Lifecycle - Overall Installation and Commissioning N/A The requirements for overall installation and commissioning do not apply to this SEooC development. N/A
Part 1: General Requirements o. Safety Lifecycle - Overall Safety Validation Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements were planned to be validated in pre-silicon and post-silicon testing. Validation and Characterization Plans
Part 1: General Requirements p. Safety Lifecycle - Overall Operation, Maintenance and Repair N/A The requirements for overall operation, maintenance and repair do not apply to this SEooC development. N/A
Part 1: General Requirements q. Safety Lifecycle - Overall Modification and Retrofit N/A The requirements for overall modification and retrofit do not apply to this SEooC development. N/A
Part 1: General Requirements r. Safety Lifecycle - Decommissioning or Disposal N/A The requirements for decommissioning or disposal do not apply to this SEooC development. N/A
Part 1: General Requirements s. Verification Pass These requirements were applied at the IC level, not the system level. IC functional safety activities have been verified by persons of appropriate independence. Verification Plans and Reports for each safety work product per Safety Plan
Part 1: General Requirements t. Functional Safety Assessment Pass Refer to section 2 for a summary of the functional safety assessment. Functional Safety Assessment
Part 2: Requirements for E/E/PE Safety-Related Systems a. E/E/PE System Design Requirements Specification Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements were generated from system assumptions. System Functional Safety Assumptions and Requirements, SRS
Part 2: Requirements for E/E/PE Safety-Related Systems b. E/E/PE System Safety Validation Planning Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements were planned to be validated in pre-silicon and post-silicon testing. Validation and Characterization Plans
Part 2: Requirements for E/E/PE Safety-Related Systems c. E/E/PE System Design & Developments Including ASICs & Software Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements were realized in the product design. Design Specification
Part 2: Requirements for E/E/PE Safety-Related Systems d. E/E/PE System Integration N/A The requirements for system integration do not apply to this SEooC development. N/A
Part 2: Requirements for E/E/PE Safety-Related Systems e. E/E/PE System Installation, Commissioning, Operation and Maintenance Procedures N/A The requirements for system installation, commissioning, operation and maintenance do not apply to this SEooC development. N/A
Part 2: Requirements for E/E/PE Safety-Related Systems f. E/E/PE System Safety Validation Pass These requirements were applied at the IC level, not the system level. IC functional safety requirements have been validated in pre-silicon and post-silicon testing. Validation and Characterization Plans and Reports
Part 2: Requirements for E/E/PE Safety-Related Systems g. E/E/PE System Modification N/A The requirements for system modification do not apply to this SEooC development. N/A
Part 2: Requirements for E/E/PE Safety-Related Systems h. E/E/PE System Verification Pass These requirements were applied at the IC level, not the system level. IC functional safety activities have been verified by persons of appropriate independence. Verification Plans and Reports for each safety work product per Safety Plan
Part 2: Requirements for E/E/PE Safety-Related Systems i. E/E/PE System Functional Safety Assessment Pass Refer to section 2 for a summary of the functional safety assessment. Functional Safety Assessment
Part 3: Software Requirements All sections N/A There are no software requirements for this SEooC development. N/A
Part 4: Definitions and Abbreviations No requirements in this part N/A There are no requirements in IEC 61508-4. N/A
Part 5: Examples of Methods for the Determination of Safety Integrity Levels No requirements in this part N/A IEC 61508-5 is an informative reference. There are no requirements in IEC 61508-5, however the analysis techniques that are recommended by this part are incorporated into the TI Functional Safety Hardware work product templates that have been used for this project. N/A
Part 6: Guidelines on the Application of IEC 61508-2 and IEC 61508-3 No requirements in this part N/A IEC 61508-6 is an informative reference. There are no requirements in IEC 61508-6, however the analysis techniques that are recommended by this part are incorporated into the TI Functional Safety Hardware work product templates that have been used for this project. N/A
Part 7: Overview of Techniques and Measures No requirements in this part N/A IEC 61508-7 is an informative reference. There are no requirements in IEC 61508-7, however the analysis techniques that are recommended by this part are incorporated into the TI Functional Safety Hardware work product templates that have been used for this project. N/A