This section of steps is applicable only if there is a need to create a bootable SD Card. Skip these steps if not applicable.
To create a bootable SD Card with the active application, follow these steps:
- Right-click the application name to open the drop-down menu and select Create Boot Image (see Figure 13-1).
- Select Zynq MP from the Architecture menu and select Import from existing BIF file option (see Figure 13-2).
The Output path shows the file location of the BOOT.bin to be generated.
- After reviewing the locations of the boot elf file, FPGA bit file, and application elf, click Create Image (see Figure 13-3).
The above step generates the BOOT.bin in the output path as selected in Figure 13-2.
- Copy BOOT.bin to a FAT16 or FAT32 formatted SD Card.
- To boot from SD Card, ensure the SW6 switch positions on the ZCU102 is as per Figure 13-4.
- With the above setting on SW6 and SD card inserted, ZCU102 can now directly boot with the application.