After the build is complete, create a new application project in Vitis. To create a new project, follow these steps:
- Right-click the Platform project, go to New, then click Application Project (see Figure 9-1).
- When the New Application Project window appears (see Figure 9-2), click Next.
- Select the newly created platform ZCU102ps and click Next (see Figure 9-3).
- Type a new application name. ZCU102ps_SPI was used as an example.
- Select standalone on microblaze_0 and click Next (see Figure 9-5).
- Select Hello World from the list of templates and click Finish (see Figure 9-6).
- A fresh C project appears on top where the actual application development can start.