To set the ZCU102 board interface for VADJ_FMC, follow these steps:
- Execute the ZCU102-Board User Interface software (available for download from Xilinx.com).
- Select the appropriate COM Port to enable communication between the onboard MSP430 of the ZCU102 and the PC. This software is required to turn on the FMC_AUX supply of 1.8 V for the FMC bank of FPGA (see Figure 15-1).
- Select the Set VADJ to 1.8 V check box (see Figure 15-2).
- Confirm the same by reading the VADJ_FMC voltage. The voltage value must be 1.80 V (see Figure 15-3).