SBAU391 December   2021 TMAG5328 , TMAG5328

 

  1.   Trademarks
  2. 1Introduction
  3. 2Assembly Guide
  4. 3 Connecting to an EVM
  5. 4 Magnetic Flux Density Results

Assembly Guide

Table 2-1 Linear Head-On Travel Attachment Table of Materials

ITEM

DESCRIPTION

QUANTITY

Screw portion of attachmentPrinted from Screw.STL file

1

Base portion of attachmentPrinted from Base.STL

1

Cylinder Magnet1/8” diameter, ½” thickness, N52 grade, axial magnetization from K&J magnetics

1

TMAG5273EVM or TMAG5170UEVM

1

Sensor Controller Board (SCB)

Control board that comes with TMAG5170UEVM and TMAG5273EVM

8333-20G

Super Glue

0.02 ounces

GUID-20211024-SS0I-XJL5-5XDH-9K4QMD4RB5VM-low.pngFigure 2-1 Linear Head-On Travel Attachment Exploded View

Step 1 – Identify the North and South Pole Faces of the Cylinder Magnet

Unipolar Hall position sensors require that the appropriate magnetic pole is applied near the top of the Hall position sensor. Applying the incorrect magnetic pole to a unipolar sensor results in an output that does not respond to the magnet’s movement. As an example, if the output of a Hall switch only responds to when a south pole of a magnet is applied near the top of the package, the output will not switch if the north pole of the magnet is brought near the top of the Hall switch’s package.

For compatibility with unipolar Hall position sensors, the user must determine the north and south poles of the magnet before the magnet is placed in the screw attachment. To determine the north and south poles of the magnet, a second magnet with known north and south poles can be applied to the attachment’s magnet. If the known south pole of the second magnet is attracted to a face of the attachment magnet, that face is the north pole of the attachment magnet. In contrast, if the known south pole of the second magnet is repulsed from a face of the attachment magnet, that face is the south pole of the attachment magnet.

Step 2 – Print the Screw Portion of the Attachment (Screw.STL)

The screw contains the cavity where the magnet will eventually be placed. Figure 2-2 and Figure 2-3 show the side and bottom view of the screw attachment. To use this attachment with other magnets, the diameter and length of the cavity can be altered by modifying the screw 3D print file.

GUID-20211024-SS0I-LJ3M-XH4H-015W39RHJDWT-low.png Figure 2-2 Side View of Screw
GUID-20211024-SS0I-Q6GT-NLRJ-0WBVMWT6CGPR-low.png Figure 2-3 Bottom View of Screw

Step 3 – Glue the Magnet into the Screw

For compatibility with south-responding unipolar Hall sensors, the south pole of the magnet must be placed above the package of the Hall sensor. This is done by inserting the north pole of the magnet, as determined from Step 1, into the cavity of the screw attachment. To ensure the magnet is secured, add glue to the north face of the magnet before inserting it into the cavity. Figure 2-4 shows the orientation of the magnet before it is inserted into the screw’s cavity.

GUID-20211024-SS0I-TW1H-JHLZ-WN8NDWHKJRFL-low.png Figure 2-4 Orientation of Magnet With Respect to Screw

After the magnet is inserted into the cavity, push the magnet down the cavity so that only a minimum amount of the magnet sticks out of the attachment, as shown in Figure 2-5. How far the magnet is actually pushed within the cavity determines the maximum magnetic flux density reading seen in the system when the screw is fully fastened in the base (see Figure 1-2). The more the magnet is pressed within the cavity, the smaller the displacement from the actual magnet to the sensor and the smaller the maximum magnetic flux density seen in the system.

GUID-20211024-SS0I-TFR7-GFKJ-4W3CD8VGZ7QH-low.png Figure 2-5 Fully-Embedded Magnet in the Screw

Leave the screw attachment unbothered until the glue fully cures after the prescribed dry time has elapsed.

Step 4 – Print the Base Portion of the Attachment (Base.STL)

The screw part of the attachment gets fastened into the top portion of the base. Figure 2-6 shows the base part of the attachment.

GUID-20211024-SS0I-4RZ0-C17T-VSQLRKSRHSBV-low.png Figure 2-6 Base of Attachment