SBAA541 December 2022 AMC1202 , AMC1302 , AMC1306M05 , AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C14 , AMC23C15 , AMC3302 , AMC3306M05
This chapter investigates offset error on the DC/DC converter. The same control-loop settings, current-sensor bandwidth of 100 kHz, and 0% gain error of the current sensor were assumed in the simulation for the settling time simulation shown in Figure 3-5. The offset error has been varied from 0%, 1%, to 2%.
Again, settling time is unaffected by offset error. The settled output current is significantly affected. For 1% offset error the current output is 1.5% or 0.3 A lower (for 2% offset the output shows 3% or 0.6 A error, respectively).
Like the Gain Error, the Offset Error is specified to the full-scale error. In our example, the full-scale current was 32 A. This means at a 1% error, the absolute error is 0.3 A (for 2%, absolute 0.6 A). The simulation indicates these results are precise.
Unlike the gain error that scales relative to the output, the offset error adds in absolute to the output current that is set in a converter. Offset error is either calibrated out or compensated by feedforward techniques (adding the known error to the output).
In summary, both gain and offset error do not impact the settling time of the control loop as long as the current sensor has a high enough bandwidth not to limit the control-loop bandwidth. Both gain and offset error impacts the accuracy of the DC-charger output. For the target specifications of the EV-Charger defined in Table 1-1, this means the current sensor needs to have a bandwidth between 10 kHz and 100 kHz and total error (for both gain and offset) smaller than 1%. Use offset calibration to achieve the target.